This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: the AM625 processor can be cascaded with SPEs using the internal switch(cpSW3G) andDP83TD510ERHBR

Part Number: AM625

if the AM625 processor can be cascaded with SPEs using the internal switch(cpSW3G) andDP83TD510ERHBR.

thanks

  • Hello,

    Yes, the AM625 processor can be cascaded with SPEs (Signal Processing Engines) using the internal switch cpSW3G and DP83TD510ERHBR. The internal switch cpSW3G allows for interconnection between multiple AM625 processors and SPEs, enabling communication and data exchange between them.

    The DP83TD510ERHBR is a Gigabit Ethernet PHY (Physical Layer) transceiver that can be used for networking connectivity. It provides the necessary Ethernet interface for connecting the AM625 processor and SPEs to an external network or other devices.

    By utilizing the internal switch and the DP83TD510ERHBR, you can create a network of interconnected AM625 processors and SPEs, enabling distributed processing and collaboration between them.

    Regards,

    Gary

  • Hello,

    You're welcome, feel free to communicate if you have any questions, thank you!

    Regards,

    Gary