This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: AM5728的使用问题----urgent

Part Number: AM5728

我们想使用AM5728 的GPMC接口, 同步,复用,16bit模式,

1. 我们按照TRM配置了寄存器,然后去读写,发现gpmc_clk都没有输出,但是通过串口打印读到的数据是0x0000,有什么建议吗?

  • 您好,

    有几个可能的原因

    1. 时钟配置错误:请确保正确配置GPMC时钟,并确保时钟源正常工作。
    2. 引脚复用设置错误:确保将相应的GPIO引脚设置为GPMC功能,并将其正确连接到外部器件。检查引脚复用配置是否正确。
    3. 信号电平不匹配:检查外部器件和AM5728之间的电平匹配是否正确。确保使用正确的电平转换电路,以便GPMC能够正常工作。
    4. GPMC配置错误:检查GPMC寄存器配置是否正确。确保所有必要的寄存器都已正确设置,包括地址映射、时序参数以及读写操作等。