你好,下载得到TDA4VH EVM的参考资料,开发板中4路uart 通过FT2232转换成micro USB接口,又保留了JTAG MIPI60还有usb的其他接口等这些调试接口。想了解一下TDA4VH-Q1的基础的必要的调试接口有哪些?因为很多复用的接口,想删除没有必要的调试接口,腾出来给外设使用。
以上,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 任意一个uart接口都可以用来打印log吗?
都可以
2. JTAG接口就是将标准的JTAG接口TRSTN\TCK\TDI\TDO\TMS五根线接出来就可以对吗?
JTAG有14pin和60pin,看您具体的设计要求。
仿真器xds110, xds560都可以。
3. evm上jtag是有拉到TM4C1294NCPDTT3R上的,是做什么用的呢?
实现板载xds110仿真功能,不用外接仿真器。
是不是就可以删除mipi-60部分的设计了?
是的。
还有个疑问EVM 上有HYPERLINK SIDEBAND CONNECTOR,这个是做什么用的?
Hyperlink是一种高速接口。