This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-TDA4VM: OSPI能当通用单线、或八线spi来收发设备数据吗?

Part Number: SK-TDA4VM


TI专家您好,最近在看pdk_jacinto_08_06_01_03这个组件下关于ospi的示例代码main_ospi_flash_test.c,

想参考此代码直接改成通用的单线或双线或四线,或8线spi读写来使用吗?  

改写的伪代码如下:

...
Board_init(boardCfg);
...
OSPI_init();
OSPI_v0_HwAttrs ospi_cfg;
OSPI_socInit();
OSPI_socGetInitCfg(SPI_OSPI_DOMAIN_MCU,peripheralNum,&ospi_cfg);
ospi_cfg.dac.dacEnable=true;
ospi_cfg.dac.dmaEnable=false;
ospi_cfg.dac.intrEnable=false;
ospi_cfg.dac.phyEnable=false;
ospi_cfg.dac.dtrEnable=false;
ospi_cfg.dac.xferLines=OSPI_XTER_LINES_SINGLE;
ospi_cfg.dac.funcClk=OSPI_MODULE_CLK_133M;
ospi_cfg.devDelays[3]=OSPI_DEV_DELAY_CSDA;

OSPI_socSetInitCfg(SPI_OSPI_DOMAIN_MCU,peripheralNum,&ospi_cfg);

OSPI_Handle * handle;
*Handle=OSPI_open(SPI_OSPI_DOMAIN_MCU);

...
//tx data
OSPI_Transaction ospiTransaction;
ospiTransaction.count = n;    /* Transfer Length */
ospiTransaction.txBuf = transmitBuffer; /* Buffer to be written */
ospiTransaction.rxBuf = NULL;  /* Buffer holding the received data */
transferOK = OSPI_transfer(ospi, &ospiTransaction); /* Perform OSPI transfer */
if (!transferOK) {
/* OSPI transaction failed */
}
对于上述代码编译并在板子上运行时,我测试时钟线时却发现多了一个字节的时钟波形,比如发送1个字节,测试却有两个字节的时钟波形,发送3个字节,有4个字节的时钟波形?
另外当我设置为八线时(ospi_cfg.dac.xferLines=OSPI_XTER_LINES_OCTAL;),写一个字节的数据是八根数据线分别传输这个字节数据的一位呢,还是一个字节只在一根数据线上传输呢?
期待您的回复,谢谢!
best wishes
Ling Wang