This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

最近在弄c6747的EDMA3的程序,只是简单从FPGA内构造的FIFO内读数据内部的RAM或者外部的SDRAM,请问在哪能下到关于C6747的官方例程



因为是初学者,看完数据手册,但是还是不知道从哪写起,请大神们指导一下,在哪能下到关于C6747的官方例程,拜托,拜托了,因为老师那边急着要了,

  • CSL_Edma3ccParamSetRegs param;  edmaInit();     param.OPT = (EDMA_EMIFA_TCC << 12) | (1 << 8) | (1 << 20)|(1 << 21); //1维数据传输,数据宽度32位,源地址增加,完成中断使能,检测中断设置为EDMA_EMIFA_TCC=5,即IPR[5]将被置为1     param.SRC = (Uint32)EMIFA_send_Add;                  //源地址,即EMIFA的发送地址     param.A_B_CNT = (1 << 16)| sample_size ;             //当设置1维时,2维计数值为1,即意味着是一维矩阵     param.DST = (Uint32)SDRAM_recevie_Add;               //目的地址,即SDRAM的接收地址     param.SRC_DST_BIDX =0x0000;                          //实现多帧数据传输时设置源索引参数(0 << 16) | ping_offset  : DSTBIDX|SCRBIDX         param.LINK_BCNTRLD = (0 << 16) | (0xffff);//(0 << 16) | (0xffff);     //当一个通道完成后链接到设置地址对应的下一个通道,如果设置0XFFFF则该通道结束后RAM里德参数全清零,只有LINK参数保持0xFFFF     param.SRC_DST_CIDX = (0 << 16)| (0x0000);          //实现多帧数据传输时设置目的索引                        |(ping_c_idx & 0x0000FFFF)   format: DSTCIDX|SRCCIDX     param.CCNT =sample_count;                            //三维计数器,当只有一帧数据时设置0x0001,sample_count                                                       //128个参数RAM,则ParamNum设置为0吧      edmaWritePaRAM(EDMA_EMIFA_PaRAM, &param);      //edmaCcRegs->IER|= (Uint32)0x1 << EDMA_EMIFA_TCC;     EdmaIntEnable(EDMA_EMIFA_TCC);                     //哪个通道对应哪个中断标志     EdmaEnableChannel(EDMA_GPIO_BANK4,0);     edmaSetEvent(EDMA_GPIO_BANK4);

  • 上面内容很乱,整理一下吧。