Other Parts Discussed in Thread: AM69A
有两个问题要提问。
1.我在Main域部署了深度学习模型,模型输出结果保存在哪里?
2.我想把输出结果从Main域传到MCU域,要怎么传输?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请看下面e2e工程师的回复。
Can you elaborate what do you mean by output here ?
Are you talking about compiled model artifacts binaries or some post processing output dump or anything else ?
2. How to transfer the output Models from Main Domain to MCU Domain?
What you trying to achieve exactly here in case ? and by the term output model what are you referring to ?
Can you reconfirm you are using TIDLRT flow and not OSRT on linux sdk you mentioned above??
This is documentation for TIDLRT which is supported as part of RTOS SDK.
This is OSRT documentation : https://github.com/TexasInstruments/edgeai-tidl-tools
请看下面e2e工程师的回复。
Okay so as I see, you are using OSRT flow (edgeai-tidl-tools) to compile and execute the model.
However there are couple of open loop questions whose answers are not clear to me.
Pasting it here again.
1. Which SDK version you are using for OSRT tools ?
2. As per posted question i can see part number listed as TDA4VH EVM, still not sure are you using AM69A Linux SDK on the same or RTOS SDK ?
3.
his curve has several parameters, such as an offset distance of 5, and I want to pass this variable to the peripheral. What should I do.
As pointed out your model is up and running on EVM, can you throw some light in understanding above statement you have ?