This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368解码输出支持数字RGB吗

TI工程师好,

       麻烦问一下,我用dm368做解码器,dm368解码输出支持数字RGB吗?如果支持,如何配置?

  • 你好,

    请问你是解码什么?视频?什么格式? 解码后是在DM36x上用LCD接口输出显示么?为什么需要RGBs输出?

  • 你好,我们解码的是H.264的文件,分辨率为720P 60,解码后直接通过DM368的数字RGB接口输出,DM368输出的后端连接的是数字RGB信号

  • 我们遇到的问题是

    我们目前遇到的问题:直接执行/usr/share/ti/dvsdk-demos的decode报错:
    root@dm368-evm:/usr/share/ti/dvsdk-demos# ./decode -v /usr/share/ti/data/videos/davincieffect.264 -y 5
    Decode demo started.
    Error: Failed to get attribute window buffer
    ARM Load: 2% Video fps: 3 fps Video bit rate: 34 kbps Sound bit rate: 0 kbps Time: 00:00:01 Demo: Decode Display: 1080I 30Hz Video Codec: H.264 HP Video Resolution: 1280x720 Sound Codec: N/A Sampling Freq: N/A

    ARM Load: 2% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 0 kbps Time: 00:00:02 Demo: Decode Display: 1080I 30Hz Video Codec: H.264 HP Video Resolution: 1280x720 Sound Codec: N/A Sampling Freq: N/A

    ARM Load: 0% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 0 kbps Time: 00:00:03 Demo: Decode Display: 1080I 30Hz Video Codec: H.264 HP Video Resolution: 1280x720 Sound Codec: N/A Sampling Freq: N/A

    ARM Load: 1% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 0 kbps Time: 00:00:04 Demo: Decode Display: 1080I 30Hz Video Codec: H.264 HP Video Resolution: 1280x720 Sound Codec: N/A Sampling Freq: N/A
    一般来说,直接执行TI的Demo,应该能够执行成功而没有输出显示,但现在直接使用TI的Demo也不对,通过调试分析TI的代码,在display.c->Display_get->Display_v4l2_get->ioctl(hDisplay->fd, VIDIOC_DQBUF, &v4l2buf)时卡死没有返回(内核卡死在stream_next_buffer->videobuf_waiton)

    麻烦问一下,这个可能的原因是什么

  • 你好,

    你有修改过OSD相关的驱动软件么?下面的错误是和OSD窗口有关的。

    Error: Failed to get attribute window buffer

  • 你好,我们没有修改过OSD相关的驱动软件

  • 你好,麻烦问一下,dm368的解码SDK包中支持解码输出24位数字RGB吗?