专家们好!
我有些问题想问一下。
- 在运行sk-tda4中edgeai-gst-apps中的demo时如何用到c66和c7的,在哪里能找到关于c66和c7的源码;
- 文件夹edgeai-tiovx-kernels和文件夹edgeai-tiovx-modules以及它们的子文件夹test的作用;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
抱歉回复晚了,请看下面e2e工程师的回复。
Thank you for your patience.
How does the edgeai-gst-apps demo use c66 and c7 core? Is there some source code for c66 and c7?
As part of edgeai sdk offering, it uses C6x and C7x binaries however the source code is not exposed.
. What is the function of edgeai-tiovx-kernels and edgeai-tiovx-modules and the test?
The gstreamer is plugin based framework we have, there are few open source plugins and few TIs TIOVX (Based on OpenVx)
The tiovx based modules/plugins enables OpenVx pipeline on TI SoC, where openvx pipeline will run on ARM core, and based on specified targets of each node it will get offloaded to it, via internal IPC mechanism.