This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 目标板执行video_copy 例程出错 求帮助?

Other Parts Discussed in Thread: OMAP3530, ADS7846, TVP5146M2

 板子用的天漠的SBC8100,OMAP3530的芯片,256M DDR SDRAM

                                                                                       256M NAND FLASH

 

DVSDK是从TI网上下载的,编译codec engine 中的 video_copy例程,在主机上可以正确编译,将相关组件放到开发板上运行出错,不知道错在哪里?

运行情况如下:

        [root@OMAP3EVM 1]# ./loadmodules.sh
CMEMK module: built on Sep 22 2009 at 10:44:38
  Reference Linux version 2.6.29
  File /db/rtree/install/trees/products/davincisw-h44x/imports/dvsdk_COMMON/dvsdk_3_00_02_44/linuxutils_2_24_02/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
ioremap_nocache(0x90000000, 50331648)=0xd3000000
allocated heap buffer 0xd3000000 of size 0x2cac000
cmem initialized 3 pools between 0x90000000 and 0x93000000
DSPLINK Module (1.61.03) created on Date: Apr 16 2009 Time: 18:31:36
mknod: /dev/dsplink: File exists
[root@OMAP3EVM 1]# ls -a
.                 app_local.xv5T    in.dat            sdmak.ko
..                app_remote.xv5T   loadmodules.sh    unloadmodules.sh
all.x64P          cmemk.ko          lpm_omap3530.ko
app_local.x64P    dsplinkk.ko       out.dat
[root@OMAP3EVM 1]# ./app_local.x64P
./app_local.x64P: line 8: syntax error: word unexpected (expecting ")")
[root@OMAP3EVM 1]# ./app_local.xv5T
@0x000971ae:[T:0x4001cfb0] ti.sdo.ce.examples.apps.video_copy.siUnhandled fault: external abort on non-linefetch (0x1818) at 0x40022000
nglecpu - main> ti.sdo.ce.examples.apps.video_copy.singlecpu
@0x000973d4:[T:0x4001cfb0] ti.sdo.ce.examples.apps.video_copy.singlecpu - App-> Application started.
Bus error
[root@OMAP3EVM 1]# ./app_remote.xv5T
@0x000b222c:[T:0x4001cfb0] ti.sdo.ce.examples.apps.video_copy.singlecpu - main> ti.sdo.ce.examples.apps.video_copy.singlecpu
@0x000b26d2:[T:0x4001cfb0] ti.sdo.ce.examples.apps.video_copy.singlecpu - App-> Application started.
Unhandled fault: external abort on non-linefetch (0x1818) at 0x4001f000

之前loadmodules.sh不能正确加载,手动修改了cmemk的地址,难道loadmodules.sh还是没有设置对? 还是别的哪方面的问题?

刚接触不久,小白一个,希望各位多多帮助!

  • 能不能贴下你的kernel boot args

  • Texas Instruments X-Loader 1.41                                                                      

    Starting OS Bootloader...

    U-Boot 1.3.3-svn (May  5 2010 - 13:10:34)

    OMAP3530-GP rev 2, CPU-OPP2 L3-165MHz

    SBC8100 Board + LPDDR/NAND

    DRAM:  256 MB

    NAND:  256 MiB

    Using default environment

    Display-bmp: 480 x 272  with 256 colors

    In:    serial

    Out:   serial

    Err:   serial

    Hit any key to stop autoboot:  0

    NAND read: device 0 offset 0x280000, size 0x300000

    3145728 bytes read: OK

    ## Booting kernel from Legacy Image at 80300000 ...

      Image Name:   Linux-2.6.29-rc3-omap1

      Image Type:   ARM Linux Kernel Image (uncompressed)

      Data Size:    2212312 Bytes =  2.1 MB

      Load Address: 80008000

      Entry Point:  80008000

      Verifying Checksum ... OK

      Loading Kernel Image ... OK

    OK

    Starting kernel ...

    Uncompressing Linux............................................................................................................................................... done, booting.

    Linux version 2.6.29-rc3-omap1 (luofc@TIOP) (gcc version 4.2.1 (CodeSourcery Sourcery G++ Lite 2007q3-51)) #1 Fri Jul 9 16:06:20 CST 2010

    CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c5387f

    CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache

    Machine: OMAP3 SBC8100

    Ignoring unrecognised tag 0x54410008

    Memory policy: ECC disabled, Data cache writeback

    OMAP3530 ES3.1 (full speed SGX, IVA2)

    SRAM: Mapped pa 0x40200000 to va 0xd7000000 size: 0x100000

    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024

    Kernel command line: console=ttyS2,115200n8 ubi.mtd=4 root=ubi0:rootfs rootfstype=ubifs video=omapfb:mode:4.3inch_LCD

    Clocking rate (Crystal/DPLL/MPU core): 26.0/266/500 MHz

    IVA2 clocking rate: 360 MHz

    Reprogramming SDRC

    dpll3_m2_clk rate change failed: -22

    GPMC revision 5.0

    IRQ: Found an INTC at 0xd8200000 (revision 4.0) with 96 interrupts

    Total of 96 interrupts on 1 active controller

    OMAP34xx GPIO hardware version 2.5

    PID hash table entries: 1024 (order: 10, 4096 bytes)

    OMAP clockevent source: GPTIMER1 at 32768 Hz

    Console: colour dummy device 80x30

    Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)

    Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)

    Memory: 128MB 128MB = 256MB total

    Memory: 254976KB available (4072K code, 371K data, 164K init)

    Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696)

    Mount-cache hash table entries: 512

    CPU: Testing write buffer coherency: ok

    net_namespace: 520 bytes

    NET: Registered protocol family 16

    omap3evmdc: Driver registration complete

    OMAP DMA hardware revision 4.0

    USB: No board-specific platform config found

    OMAP DSS rev 2.0

    OMAP DISPC rev 3.0

    OMAP VENC rev 2

    OMAP DSI rev 1.0

    bio: create slab <bio-0> at 0

    i2c_omap i2c_omap.1: bus 1 rev3.12 at 2600 kHz

    twl4030: PIH (irq 7) chaining IRQs 368..375

    twl4030: power (irq 373) chaining IRQs 376..383

    twl4030: gpio (irq 368) chaining IRQs 384..401

    i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz

    i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz

    SCSI subsystem initialized

    twl4030_usb twl4030_usb: Initialized TWL4030 USB module

    usbcore: registered new interface driver usbfs

    usbcore: registered new interface driver hub

    usbcore: registered new device driver usb

    musb_hdrc: version 6.0, musb-dma, peripheral, debug=0

    musb_hdrc: USB Peripheral mode controller at d80ab000 using DMA, IRQ 92

    NET: Registered protocol family 2

    IP route cache hash table entries: 2048 (order: 1, 8192 bytes)

    TCP established hash table entries: 8192 (order: 4, 65536 bytes)

    TCP bind hash table entries: 8192 (order: 3, 32768 bytes)

    TCP: Hash tables configured (established 8192 bind 8192)

    TCP reno registered

    NET: Registered protocol family 1

    OMAP35x Linux PSP version 02.01.03.11 (OMAP3EVM)

    NetWinder Floating Point Emulator V0.97 (double precision)

    VFS: Disk quotas dquot_6.5.2

    Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

    JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.

    msgmni has been set to 498

    alg: No test for stdrng (krng)

    io scheduler noop registered

    io scheduler anticipatory registered (default)

    io scheduler deadline registered

    io scheduler cfq registered

    Generic Backlight Driver Initialized.

    Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

    serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654

    serial8250.0: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654

    serial8250.0: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654

    console [ttyS2] enabled

    brd: module loaded

    loop: module loaded

    dm9000 Ethernet Driver, V1.31

    eth0 (dm9000): not using net_device_ops yet

    eth0: dm9000a at d08b2000,d08b6400 IRQ 185 MAC: 00:11:22:33:44:55 (chip)

    Linux video capture interface: v2.00

    tvp514x 2-005d: Registered to v4l2 master omap34xxcam!!

    usbcore: registered new interface driver uvcvideo

    USB Video Class driver (v0.1.0)

    i2c /dev entries driver

    Driver 'sd' needs updating - please use bus_type methods

    omap2-nand driver initializing

    NAND device: Manufacturer ID: 0x2c, Chip ID: 0xba (Micron NAND 256MiB 1,8V 16-bit)

    Creating 5 MTD partitions on "omap2-nand.0":

    0x000000000000-0x000000080000 : "X-Loader"

    0x000000080000-0x000000260000 : "U-Boot"

    0x000000260000-0x000000280000 : "U-Boot Env"

    0x000000280000-0x000000680000 : "Kernel"

    0x000000680000-0x000010000000 : "File System"

    UBI: attaching mtd4 to ubi0

    UBI: physical eraseblock size:   131072 bytes (128 KiB)

    UBI: logical eraseblock size:    129024 bytes

    UBI: smallest flash I/O unit:    2048

    UBI: sub-page size:              512

    UBI: VID header offset:          512 (aligned 512)

    UBI: data offset:                2048

    UBI: attached mtd4 to ubi0

    UBI: MTD device name:            "File System"

    UBI: MTD device size:            249 MiB

    UBI: number of good PEBs:        1996

    UBI: number of bad PEBs:         0

    UBI: max. allowed volumes:       128

    UBI: wear-leveling threshold:    4096

    UBI: number of internal volumes: 1

    UBI: number of user volumes:     1

    UBI: available PEBs:             0

    UBI: total number of reserved PEBs: 1996

    UBI: number of PEBs reserved for bad PEB handling: 19

    UBI: max/mean erase counter: 2/1

    usbmon: debugfs is not available

    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

    ehci-omap ehci-omap.0: OMAP-EHCI Host Controller

    UBI: background thread "ubi_bgt0d" started, PID 407

    ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1

    ehci-omap ehci-omap.0: irq 77, io mem 0x48064800

    ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00

    usb usb1: configuration #1 chosen from 1 choice

    hub 1-0:1.0: USB hub found

    hub 1-0:1.0: 3 ports detected

    Initializing USB Mass Storage driver...

    usbcore: registered new interface driver usb-storage

    USB Mass Storage support registered.

    g_ether gadget: using random self ethernet address

    g_ether gadget: using random host ethernet address

    usb0: MAC f2:c2:9b:db:f0:48

    usb0: HOST MAC ba:a2:7a:a9:2a:8c

    g_ether gadget: Ethernet Gadget, version: Memorial Day 2008

    g_ether gadget: g_ether ready

    input: omap_twl4030keypad as /class/input/input0

    ads7846 spi2.0: touchscreen, irq 187

    input: ADS784x Touchscreen as /class/input/input1

    twl4030_rtc twl4030_rtc: rtc core: registered twl4030_rtc as rtc0

    twl4030_rtc twl4030_rtc: Power up reset detected.

    twl4030_rtc twl4030_rtc: Enabling TWL4030-RTC.

    OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec

    cpuidle: using governor ladder

    cpuidle: using governor menu

    register sdio_ti_driver is OK!

    Registered led device: led0

    Registered led device: led1

    usb 1-1: new high speed USB device using ehci-omap and address 2

    Registered led device: led2

    mmc1: new SDIO card at address 0001

    Registered led device: led3

    ti_sdio_probe: Add glue driver

    usbcore: registered new interface driver usbhid

    usbhid: v2.6:USB HID core driver

    Advanced Linux Sound Architecture Driver Version 1.0.19.

    No device for DAI twl4030

    No device for DAI twl4030 Voice

    No device for DAI omap-mcbsp-dai-0

    No device for DAI omap-mcbsp-dai-1

    No device for DAI omap-mcbsp-dai-2

    No device for DAI omap-mcbsp-dai-3

    No device for DAI omap-mcbsp-dai-4

    TWL4030 Audio Codec init

    asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok

    usb 1-1: config 1 has an invalid descriptor of length 0, skipping remainder of the config

    usb 1-1: config 1 interface 0 altsetting 1 has 0 endpoint descriptors, different from the interface descriptor's value: 1

    ALSA device list:

     #0: omap3evm (twl4030)

    TCP cubic registered

    NET: Registered protocol family 17

    NET: Registered protocol family 15

    RPC: Registered udp transport module.

    RPC: Registered tcp transport module.

    Power Management for TI OMAP3.

    usb 1-1: configuration #1 chosen from 1 choice

    hub 1-1:1.0: USB hub found

    hub 1-1:1.0: 4 ports detected

    SmartReflex driver initialized

    VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1

    omapfb: using mode 4.3inch_LCD

    Console: switching to colour frame buffer device 60x34

    GPIO-153 autorequested

    omap-dss DISPC error: Requested pixel clock not possible with the current OMAP2_DSS_MIN_FCK_PER_PCK setting. Turning the constraint off.

    tvp514x 2-005d: tvp5146m2 found at 0xba (OMAP I2C adapter)

    hub 1-1:1.0: activate --> -2

    omap34xxcam omap34xxcam: video0 is now omap3/tvp514x//

    Display already enabled

    Display already enabled

    Buffer Size = 3686400

    omap_vout: registered and initialized                   video device 1 [v4l2]

    Buffer Size = 3686400

    omap_vout: registered and initialized                   video device 2 [v4l2]

    display->updated

    twl4030_rtc twl4030_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)

    UBIFS: recovery needed

    UBIFS: recovery completed

    UBIFS: mounted UBI device 0, volume 0, name "rootfs"

    UBIFS: file system size:   103348224 bytes (100926 KiB, 98 MiB, 801 LEBs)

    UBIFS: journal size:       9033728 bytes (8822 KiB, 8 MiB, 71 LEBs)

    UBIFS: media format:       4 (latest is 4)

    UBIFS: default compressor: lzo

    UBIFS: reserved for root:  0 bytes (0 KiB)

    VFS: Mounted root (ubifs filesystem) on device 252:1.

    Freeing init memory: 164K

    init started: BusyBox v1.9.1 (2008-10-17 18:20:44 IST)

    starting pid 482, tty '': '/etc/init.d/rcS'

       System initialization...

       Hostname       : OMAP3EVM

       Filesystem     : v1.0.2

       Kernel release : Linux 2.6.29-rc3-omap1

       Kernel version : #1 Fri Jul 9 16:06:20 CST 2010

    Mounting /proc             : [SUCCESS]

    Mounting /sys              : [SUCCESS]

    Mounting /dev              : [SUCCESS]

    Mounting /dev/pts          : [SUCCESS]

    Enabling hot-plug          : [SUCCESS]

    Populating /dev            : [SUCCESS]

    Mounting other filesystems : [SUCCESS]

    Starting syslogd           : [SUCCESS]

    Starting telnetd           : Jan  1 00:00:01 OMAP3EVM syslog.info syslogd started: BusyBox v1.9.1

    [SUCCESS]

    eth0: link down

    System initialization complete.

    start aging test...

    interval = 86400 second

    Please press Enter to activate this console.

  • 这是板子上NAND FLASH固化的嵌入式Linux,会不会这个板子上的Linux系统不合适?需要特定的Linux,比如MontaVista Linux什么的?

  • 我看了下,板子上固化的Linux,使用了整个0x80000000~0x90000000 的空间,我给cmem的地址,是在0x9000000以后的地址段分配的,是不是这也是不对的?大致要怎么改呢,特别是板子上的Linux要怎么改吗?谢谢了!

  • 你好,我觉得你这个问题应该就是arm和dsp的cmem共享内存地址分配错误了,呵呵dvsdk单单在linux比起在android下使用简单多了,你的地址分配 loadmodules.sh 可以参考dvsdk目录下面的/dvsdk/codec-engine_2_26_02_11/examples/apps/system_files/OMAP3530/,然后关键是设好botargs 中的mem,我的

    mem=68M@0x80000000 mem=128M@0x88000000,预留了60M给dsp和arm共享通信,实际在loadmodules,sh申请了大概是10M,希望对你有帮助

    可以参考http://community.csdn.net/

  • 忘了说下我的内存也是256M ,0x8到0x9也就刚好256,所以你去外面申请当然没用根本没有空间了啊,这个我之前也干过这种傻事

  • botargs 中的mem 在哪设置,是在开发板的源码里吗? 那需要重新编译内核并烧到板子上吗?

  • 谢谢了,呵呵!刚接触,好多都不了解~

  • 这个在uboot启动的参数设置啊,没弄过吗

  • 网上搜了下,知道怎么设置了,谢了呵

  • 你是怎么设置的啊

  • 不好意思,我想问下,你是怎么设置botargs中的mem的

  • 参考TI的官网bootargs