This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127中DSP读取外存数据提速的问题



最近尝试使用DM8127中的DSP开发一些图象的增强算法,但在测试过程中发现,由于DSP读取视频帧数据耗时过多,导致实时性难以保证。

一个简单的测试是,对主码流(1920x1080)中的Y分量:(1)遍历赋值为255,耗时10ms左右;(2)遍历取值操作,耗时12ms左右。在DSP中定义全局变量来进行上述操作,耗时也一样。可见只对Y分量进行一次存取操作,耗时就在20ms以上,如果要进行RGB三个通道的操作,已经无法满足实时性了。

请问一下,应该如何提高DSP访问外存的速度,以保证在DSP中可完成对主码流的增强处理?