Part Number: AM625
你好:
在emmc启动中。可以通过ls mmc 0:1命令查询rootfs分区和文件想问一下如何查看boot0和boot1这两个分区呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请看下面e2e工程师的回复。
The SDK User's Guide has some explanation on this, see https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/09_00_00_03/exports/docs/linux/Foundational_Components/U-Boot/UG-Memory.html#booting-tiboot3-bin-tispl-bin-and-u-boot-img-from-emmc-boot-partition-for-k3-class-of-socs
Basically, you can switch to the boot0 partition using the `mmc dev 0 1` command, and then you can access the data (in raw format, because there's no filesystem!) using the usual `mmc read` and `mmc write commands. Similarly, for accessing the boot1 partition, first switch to that partition using `mmc dev 0 2`, before doing any raw access.
请看下面e2e工程师的回复。
The last zero in the `mmc dev 0 0` command used as the parameter for the partition refers to the user data partition/area (also known as UDA). If you don't specify this last partition parameter it actually defaults to `0` so usually it is not specified at all in this case.