This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何才能让XDS560V2工作?

自己画了一块6678的板子,设计阶段考虑不够慎重,调试器选用了EVM带的XDS560V2的子卡,因此在自己的板子上对照EVM设计,留了对应的60pin的连接器座子以及6pin的电源座子。板子上没有留XDS100调试器,现在XDS560V2插在板子上,子卡不能工作,电脑无法识别,不知如何才能让XDS560V2工作?

我测了下对应的几个供电管脚电压,VCC3V3_AUX,我的大概是3.6V;VCC5我用的电压源供电,大概4.4V,使能脚我看到EVM说明文档上写到:

XDS560_IL control
0 : Disable XDS560 mezzanine card
1 : Enable XDS560 mezzanine card (Default)

但是我实际测了一下EVM板上插上XDS560V2子卡后的使能脚XDS560_IL电平,是低电平,与手册描述不符。看了下FPGA的代码,也没能弄明白。不知道子卡需要如何才能进入工作状态?

我的板子没有用FPGA,是用单片机控制对应的使能脚。我分别试了下在上电后,将该脚置高、置低,都没能使子卡工作,现象是是3个LED灯(D1,D2,D3)闪烁

另外电脑的驱动安装正常,EVM插上子卡能用。