你好:
关于DRA821U,有以下几个问题请教:
1. DRA821U的NOR Flash和NAND Flash的寻址空间是多少?能同时支持NOR Flash和NAND Flash吗?我们想用NOR Flash作为boot存储器,NAND Flash用作程序存储器。
2. DRA821U是否支持LPDDR4X。因为LPDDR4芯片容量大都为32Gb,如果需要64Gb,采用LPDDR4X是否可行?
3. DRA821U可否支持Linux操作系统。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
关于DRA821U,有以下几个问题请教:
1. DRA821U的NOR Flash和NAND Flash的寻址空间是多少?能同时支持NOR Flash和NAND Flash吗?我们想用NOR Flash作为boot存储器,NAND Flash用作程序存储器。
2. DRA821U是否支持LPDDR4X。因为LPDDR4芯片容量大都为32Gb,如果需要64Gb,采用LPDDR4X是否可行?
3. DRA821U可否支持Linux操作系统。
谢谢!
您好,
关于DRA821U的问题,以下是回答:
1. DRA821U支持多种存储器接口,包括NOR Flash和NAND Flash。具体的寻址空间大小取决于所选择的存储器芯片的容量。DRA821U可以同时支持NOR Flash和NAND Flash,因此您可以将NOR Flash用作boot存储器,将NAND Flash用作程序存储器。
2. DRA821U支持LPDDR4和LPDDR4X内存接口。LPDDR4X是LPDDR4的低功耗版本,具有更低的工作电压。关于容量,LPDDR4和LPDDR4X都支持高达16Gb的单个芯片容量。如果您需要64Gb的容量,可以通过多个LPDDR4或LPDDR4X芯片进行组合来实现。
3. DRA821U可以支持Linux操作系统。