This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678的boot模式和默认输入时钟有无关系?

手册Table 2-13中,bootmode[12:10]决定了pll的默认设置,而这个bootmode[12:10]是决定boot模式,二者是否有影响?

比如core 时钟使用的是100MHz,并且选择从spi nor flash boot 。

此时那SPI boot mode pin[12:0]应该为0b0101000000110。但是按照此时的bootmode[12:10],输入时钟为80MHz。

这个时候外部时钟是否必须要调整为80MHz?感觉不应该这样。还是哪里理解有误?

谢谢!

  • 需要根据外部输入时钟来配置pll对应的bootpin,你的理解是对的,对于010时外部输入时钟是80MHz,但是如手册所述对于SPI boot RBL不会读取bootpin来配置PLL,其中12~10的定义见手册。