This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: tda4vm+ox03c decompanding issue

Part Number: TDA4VM

Hi TI expert,

I am tuning ox03c+tda4,but i don't konw the method waht the dcc tool decompanding knee generate to OX03CC_wdr_decompand_dcc.xml and  OX03CC_lut_wdr_overall_pwl_global.txt

Can you tell me the tuning tool decompanding para  how to convert to OX03CC_wdr_decompand_dcc.xml and  OX03CC_lut_wdr_overall_pwl_global.txt,thank you!

Best Regards,

Renhui

  • add attatchments

  • Hello,

    Typically, the decompanding process involves converting the raw sensor data into a linear or perceptually uniform space. 

    Regards,

    Gary

  • Hello,

    Maybe I didn't explain the problem clearly,my question is the dcc tool how to generate the xml and pwl.txt ,How does it change in the middle. Becasue i can not  confirm that decompamding knee i fill in DCC wdr moudle correspond to the code is right?

  • I don't find the rule in the convert,thanks 

    Best Regards,

    Renhui

  • Hello,

    I see, thank you for clarifying your question.

    The dcc tool generates the XML and PWL files based on the input DCC configuration file and the source code of the software running on the target device. The XML file contains the register settings for the DCC module, while the PWL file contains the pulse width modulation (PWM) values for the DCC module.

    To ensure that the DCC configuration is correct, you need to make sure that the DCC settings in the source code match the settings in the DCC configuration file. You can use the dcc tool to generate the XML and PWL files, and then compare the generated files with the DCC configuration file and the source code to verify that they match.

    In general, when using the DCC module, it is important to carefully test and verify the configuration to ensure that it is working as expected. This may involve running tests and analyzing the output of the DCC module to confirm that it is producing the desired results.

    Regards,

    Gary

  • Hi Gary,

    Good morning,thanks for your kindly answer.It solved my question.

    Best Regards,

    Renhui