Part Number: AM5708
您好:
请问GPIO_setCallback,GPIO_setConfig等这些函数的说明文档有吗?不知道函数的功能是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
GPIO_setCallback函数用于设置一个回调函数,当GPIO引脚的状态发生变化时,该回调函数将被调用。回调函数可以是用户自定义的函数,用于处理GPIO引脚状态变化时的逻辑。通过设置回调函数,您可以实现在GPIO引脚状态变化时执行特定的操作或触发相应的事件。
GPIO_setConfig函数用于配置GPIO引脚的工作模式、输入输出方向、上下拉电阻等。通过该函数,您可以设置GPIO引脚为输入模式或输出模式,并指定相应的电平状态。您还可以设置引脚的上拉或下拉电阻,以确保引脚在无输入时保持稳定的状态。
通过GPIO_setConfig函数,您还可以配置GPIO引脚的中断功能。您可以选择在GPIO引脚状态变化时触发中断,并指定中断的触发条件(例如上升沿、下降沿、双边沿等)。当满足中断触发条件时,系统将调用设置的回调函数。
您好:为您提供技术手册:www.ti.com.cn/.../spruhz7j.pdf
您好,此文档中已含全部相关数据,为您提供此链接: