This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在vision_apps的vision_apps\platform\j721e\rtos\mcu2_0目录下main.c,里增加了SPI1的操作,但是整个进程会卡在SPI_open这里,无法执行下去,以下是我增加的操作的SPI的代码:
void spi_open(uint32_t instance,uint32_t domain) { SPI_Handle spi; SPI_Params spiParams; // uint32_t instance, domain; //domain = 1; //instance = 1; SPI_HWAttrs spi_cfg; appLogPrintf("spi_open instance=%d,domain=%d enter........\n",instance,domain); SPI_init(); SPI_socGetInitCfg(domain, instance, &spi_cfg); appLogPrintf("spi_open instance=%d,domain=%d spi_cfg.intNum=%d........\n",instance,domain,spi_cfg.intNum); spi_cfg.enableIntr = true; spi_cfg.edmaHandle = NULL; spi_cfg.dmaMode = FALSE; spi_cfg.chnCfg[0].dataLineCommMode = MCSPI_DATA_LINE_COMM_MODE_4; SPI_socSetInitCfg(domain, instance, &spi_cfg); SPI_Params_init(&spiParams); spiParams.transferMode = SPI_MODE_BLOCKING; spiParams.transferCallbackFxn = NULL; spiParams.frameFormat=SPI_POL0_PHA1; spiParams.transferTimeout = 0; spiParams.mode = SPI_MASTER; appLogPrintf("SPI_Params_init after........\n"); //memcpy(&spiParams,&SPI_defaultParams,sizeof(SPI_Params)); spi = SPI_open(domain, instance, &spiParams); if (spi == NULL) { appLogPrintf("Error initializing SPI\n"); // goto Err; } else { appLogPrintf("SPI_%d initializing......\n",instance); } }
从LOG来看是进入SPI_open后没有出来,能否帮忙看看是不是代码上有什么问题导致的?
SDK版本:ti-processor-sdk-rtos-j721e-evm-08_05_00_11
请回复一下e2e工程师的问题,谢谢!
Can you please share more details. Where exactly the code is getting stuck in SPI open. Can you please share the call trace?
Also, are you referring to any existing example in PDK for this?