各位专家好!
我现在利用EDMA从EMIF往外传输数据,想利用GPIO口的中断来作为触发事件触发EDMA传输,请问:
(1)GPIO口和EMIF是怎么样的连接关系?
(2)GPIO[0:15]中应该利用哪个端口的中断来触发,是否任意端口都可以用?
(3)应该怎么样对GIPO口进行配置?具体的说,应该配置端口为输入还是输出?
非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
1)GPIO和EMIF没有关联,GPIO应该与EDMA3关联,关联方式如楼上所示;
2)GPIO的16个pin脚都可以用,这样根据你的EVM板的设计,因为GPIO某些pin脚已经被用作其它的,因此建议使用一些没有用作特殊用途的pin脚;
3)你需要通过GPIO触发EMDA3,因此GPIO应该设置为输入,这样你可以从外部输入信号触发。