This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5708: GPIO_setCallback()函数

Part Number: AM5708


您好:

       现在用AM5708芯片,配置GPIO6_20中断函数,使用void GPIO_setCallback(uint32_t index, GPIO_CallbackFxn callback)函数,请问index是多少呢?怎么对应的呢?

     

  • 在AM5708芯片中,GPIO6_20对应的index是144。以下示例代码来配置GPIO6_20中断函数并对应callback函数:

    #include <ti/drivers/gpio/GPIO.h>
    
    void gpioCallbackFxn(uint_least8_t index)
    {
    // Your callback function implementation
    }
    
    int main()
    {
    GPIO_init();
    
    GPIO_setCallback(144, gpioCallbackFxn);
    
    // Other initialization and code
    }

    在上面的例子中,我们使用了GPIO_setCallback函数来配置GPIO6_20的中断回调函数,并将其对应的index设置为144。然后在main函数中,我们初始化GPIO并将gpioCallbackFxn函数作为回调函数传递给GPIO_setCallback函数。这样当GPIO6_20产生中断时,gpioCallbackFxn函数将被调用。