This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM:如何通过SPL拉起mcu1_0核mcusw mcal_drv

Part Number: TDA4VM

您好,

我想在A72运行linux的同时也在mcu1_0上启动运行SDK中mcusw->mcal_drv->examples->Can的提供的示例代码,我看官方提供了spl的方式8.3.MCU1_0 使用 SYSFW 进行应用程序开发 — 处理器 SDK RTOS J721E但是我按照文档操作后仍然无法启动,我不知道mcal_drv的例子是需要增加SYSFW固件启动么?  可以为我修改提供帮助么

1.我在makefile中,修改DM的路径

2.我make u-boot 后替换了sysfw.itb tiboot3.bin tispl.bin u-boot.img文件到boot

3.我修改了软连接如下 j7-mcu-r5f0_0-fw -> TDA4_R5_app_mcu1_0_release_strip.xer5f

但系统无法启动,日志如下

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
U-Boot SPL 2021.01 (Nov 14 2023 - 09:20:40 +0800)
Model: Texas Instruments J721E SK R5
Board: J721EX-EAIK rev A1
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
Trying to boot from MMC2
Starting ATF on ARM64 core...
NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE: BL31: Built : 22:56:45, Mar 3 2023
I/TC:
I/TC: OP-TEE version: 3.20.0 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Fri Mar 3 22:59:24 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
I/TC: HUK Initialized
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 sa2ul_init:59 Failed to get SA2UL device
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX