Part Number: AM5728
您好, AM5728通过IPC,将数据从DSP核搬到ARM核的物理途径,是通过AM5728片内的sram?还是通过外接的DDR3?另外哪种搬运数据的方式是通过片内ram?哪种方式是借助ddr3?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5728
您好, AM5728通过IPC,将数据从DSP核搬到ARM核的物理途径,是通过AM5728片内的sram?还是通过外接的DDR3?另外哪种搬运数据的方式是通过片内ram?哪种方式是借助ddr3?谢谢
AM5728处理器通过IPC将数据从DSP核搬到ARM核的物理途径通常是通过片内的SRAM。
另一方面,AM5728处理器也可以通过外接的DDR3内存来进行数据传输。DDR3是一种动态随机存取存储器,通常用作主存储器,具有较大的容量和较慢的访问速度,相对于SRAM来说延迟较高。
因此,通过片内的SRAM进行数据传输是一种更快速和低延迟的方式,而借助外接的DDR3进行数据传输则适合于需要大容量存储的场景。
总的来说,对于AM5728处理器,通过IPC将数据从DSP核搬到ARM核的物理途径通常会使用片内的SRAM,而外接的DDR3内存则更适合用于存储大容量数据。