This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: 我用的AM64X,请问如何设置定时器的工作模式

Part Number: AM6442
Other Parts Discussed in Thread: SYSCONFIG

我想要把一个定时器设置为向上计数模式,到达最大值自动重装载,但是我看sysconfig里面没有关于设置定时器工作模式的选项,所以我该如何设置?有没有这样的demo?

  • 在AM64X系列芯片中,定时器的工作模式可以通过寄存器配置来实现,而不是通过sysconfig进行设置。

    下面是一个简单的示例代码,演示如何在AM64X芯片上使用C语言和寄存器配置来设置定时器的工作模式为向上计数模式并启用自动重载:

    #include <stdint.h>
    #include <ti/csl/csl_timer.h>
    
    void configureTimer()
    {
    CSL_timerRegs *timer = (CSL_timerRegs *)0xADDRESS_OF_YOUR_TIMER_MODULE; // 替换为你的定时器模块的地址
    
    // 停止定时器
    timer->TIM12_TCLR &= ~CSL_TIMER_TIM12_TCLR_ST;
    
    // 设置定时器模式为向上计数模式
    timer->TIM12_TCLR &= ~CSL_TIMER_TIM12_TCLR_CE;
    timer->TIM12_TCLR &= ~CSL_TIMER_TIM12_TCLR_AR;
    timer->TIM12_TCLR |= CSL_TIMER_TIM12_TCLR_PTV(0); // 设置预分频器值
    
    // 启用自动重载
    timer->TIM12_TCLR |= CSL_TIMER_TIM12_TCLR_CE;
    timer->TIM12_TCLR |= CSL_TIMER_TIM12_TCLR_AR;
    
    // 启动定时器
    timer->TIM12_TCLR |= CSL_TIMER_TIM12_TCLR_ST;
    }

    请将示例代码中的`0xADDRESS_OF_YOUR_TIMER_MODULE`替换为您的定时器模块的基地址。