Part Number: PROCESSOR-SDK-J784S4
tda4vh运行着sdk9.0的包,当替换了自己重新编译的内核后,无法通过cat /sys/class/remoteproc/remoteproc*/name看到其他核,而使用prebuil的Image,则可以
以下是编译命令:
make ARCH=arm64 CROSS_COMPILE=aarch64-none-linux-gnu- distclean make ARCH=arm64 CROSS_COMPILE=aarch64-none-linux-gnu- defconfig ti_arm64_prune.config make -j12 ARCH=arm64 CROSS_COMPILE=aarch64-none-linux-gnu- Image
编译完成后,将arch/arm64/boot/Image拷贝到TDA4VH下的/boot目录中,然后重启。重启后,无法通过cat /sys/class/remoteproc/remoteproc*/name看到其他核。
以下是开机日志:
U-Boot SPL 2021.01-dirty (Nov 23 2023 - 16:43:35 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)')
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if td
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if td
U-Boot 2023.04-g756ba776d4 (Jul 13 2023 - 05:36:12 +0000)
SoC: J784S4 SR1.0 GP
Model: Texas Instruments J784S4 EVM
Board: J784S4X-EVM rev E2
DRAM: 32 GiB
idle-statesCore: 88 devices, 31 uclasses, devicetree: separate
Flash: 0 Bytes
MMC: mmc@4f80000: 0, mmc@4fb0000: 1
Loading Environment from nowhere... OK
In: serial@2880000
Out: serial@2880000
Err: serial@2880000
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA02102 cpsw_ver: 0x6BA82102 ale_ver: 0x00293904 Ports:1 mdio_freq:0
Unidentified board claims J784S4X-EVM in eeprom header
Net: eth0: ethernet@46000000port@1
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
743 bytes read in 27 ms (26.4 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
1 bytes read in 27 ms (0 Bytes/s)
Already setup.
## Error: "main_cpsw0_qsgmii_phyinit" not defined
k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work
1555864 bytes read in 46 ms (32.3 MiB/s)
Load Remote Processor 2 with data@addr=0x82000000 1555864 bytes: Success!
400444 bytes read in 34 ms (11.2 MiB/s)
Load Remote Processor 3 with data@addr=0x82000000 400444 bytes: Success!
191564 bytes read in 32 ms (5.7 MiB/s)
Load Remote Processor 4 with data@addr=0x82000000 191564 bytes: Success!
191564 bytes read in 32 ms (5.7 MiB/s)
Load Remote Processor 5 with data@addr=0x82000000 191564 bytes: Success!
547820 bytes read in 35 ms (14.9 MiB/s)
Load Remote Processor 6 with data@addr=0x82000000 547820 bytes: Success!
191564 bytes read in 32 ms (5.7 MiB/s)
Load Remote Processor 7 with data@addr=0x82000000 191564 bytes: Success!
14815504 bytes read in 182 ms (77.6 MiB/s)
Load Remote Processor 8 with data@addr=0x82000000 14815504 bytes: Success!
15208720 bytes read in 186 ms (78 MiB/s)
Load Remote Processor 9 with data@addr=0x82000000 15208720 bytes: Success!
14815504 bytes read in 182 ms (77.6 MiB/s)
Load Remote Processor 10 with data@addr=0x82000000 14815504 bytes: Success!
14815504 bytes read in 182 ms (77.6 MiB/s)
Load Remote Processor 11 with data@addr=0x82000000 14815504 bytes: Success!
20986368 bytes read in 244 ms (82 MiB/s)
103302 bytes read in 29 ms (3.4 MiB/s)
Working FDT set to 88000000
3935 bytes read in 28 ms (136.7 KiB/s)
14780 bytes read in 28 ms (514.6 KiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
ERROR: reserving fdt memory region failed (addr=880000000 size=80000000 flags=4)
Loading Device Tree to 000000008fee3000, end 000000008fffffff ... OK
Working FDT set to 8fee3000
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[ 0.000000] Linux version 6.1.46-dirty (yuhang@csp) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Archite3
[ 0.000000] Machine model: Texas Instruments J784S4 EVM
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002880000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a8000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a8100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000aa000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@aa000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000aa100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@aa100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ac000000, size 48 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-rtos-ipc-memory-region@ac000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000af000000, size 80 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@af000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b4000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@b4000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b4100000, size 47 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71_0-memory@b4100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b7000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71_1-dma-memory@b7000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b7100000, size 47 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71_1-memory@b7100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ba000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71_2-dma-memory@ba000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000ba100000, size 47 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71_2-memory@ba100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000bd000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71_3-dma-memory@bd000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000bd100000, size 47 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71_3-memory@bd100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000e0000000, size 80 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@e0000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000e5000000, size 8 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-queues@e5000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000e5800000, size 24 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-buffers@e5800000, compatible id shared-dma-pol
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 2048 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000980000000, size 1792 MiB
[ 0.000000] OF: reserved mem: initialized node linux-cma-buffers@980000000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x0000000fffffefff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff]
[ 0.000000] node 0: [mem 0x000000009e800000-0x00000000bfffffff]
[ 0.000000] node 0: [mem 0x00000000c0000000-0x00000000dfffffff]
[ 0.000000] node 0: [mem 0x00000000e0000000-0x00000000e6ffffff]
[ 0.000000] node 0: [mem 0x00000000e7000000-0x00000000ffffefff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000008ffffffff]
[ 0.000000] node 0: [mem 0x0000000900000000-0x0000000fffffefff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x0000000fffffefff]
[ 0.000000] On node 0, zone Normal: 1 pages in unavailable ranges
[ 0.000000] On node 0, zone Normal: 1 pages in unavailable ranges
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.4
[ 0.000000] percpu: Embedded 19 pages/cpu s38376 r8192 d31256 u77824
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: Spectre-v3a
[ 0.000000] CPU features: detected: Spectre-BHB
[ 0.000000] CPU features: detected: ARM erratum 1742098
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 8257534
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02880000 root=PARTUUID=9bc8b883-02 rwt
[ 0.000000] Dentry cache hash table entries: 4194304 (order: 13, 33554432 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 2097152 (order: 12, 16777216 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: area num 8.
[ 0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB)
[ 0.000000] Memory: 27712128K/33554424K available (12544K kernel code, 1294K rwdata, 4364K rodata, 2176K init, 498K bss,)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=8, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=8.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=8
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: [Firmware Bug]: GICR region 0x0000000001900000 has overlapping address
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @920800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000000920050000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000920060000
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008407] Console: colour dummy device 80x25
[ 0.012974] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023645] pid_max: default: 32768 minimum: 301
[ 0.028387] LSM: Security Framework initializing
[ 0.033202] Mount-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.041002] Mountpoint-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.050116] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.057515] cblist_init_generic: Setting shift to 3 and lim to 1.
[ 0.063777] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.071162] cblist_init_generic: Setting shift to 3 and lim to 1.
[ 0.077465] rcu: Hierarchical SRCU implementation.
[ 0.082361] rcu: Max phase no-delay instances is 1000.
[ 0.087844] Platform MSI: msi-controller@1820000 domain created
[ 0.094024] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.103779] EFI services will not be available.
[ 0.108612] smp: Bringing up secondary CPUs ...
WARNING: GTC: Debug access doesn't stop time. Fix Bootloader
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
WARNING: GTC: Debug access doesn't stop time. Fix Bootloader
I/TC: Secondary CPU 2 initializing
I/TC: Secondary CPU 2 switching to normal world boot
WARNING: GTC: Debug access doesn't stop time. Fix Bootloader
I/TC: Secondary CPU 3 initializing
I/TC: Secondary CPU 3 switching to normal world boot
WARNING: GTC: Debug access doesn't stop time. Fix Bootloader
I/TC: Secondary CPU 2 initializing
I/TC: Secondary CPU 2 switching to normal world boot
WARNING: GTC: Debug access doesn't stop time. Fix Bootloader
I/TC: Secondary CPU 3 initializing
I/TC: Secondary CPU 3 switching to normal world boot
WARNING: GTC: Debug access doesn't stop time. Fix Bootloader
I/TC: Secondary CPU 4 initializing
I/TC: Secondary CPU 4 switching to normal world boot
WARNING: GTC: Debug access doesn't stop time. Fix Bootloader
I/TC: Secondary CPU 5 initializing
I/TC: Secondary CPU 5 switching to normal world boot
[ 0.127181] Detected PIPT I-cache on CPU1
[ 0.127228] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[ 0.127241] GICv3: CPU1: using allocated LPI pending table @0x0000000920070000
[ 0.127273] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[ 0.141245] Detected PIPT I-cache on CPU2
[ 0.141288] GICv3: CPU2: found redistributor 2 region 0:0x0000000001940000
[ 0.141301] GICv3: CPU2: using allocated LPI pending table @0x0000000920080000
[ 0.141324] CPU2: Booted secondary processor 0x0000000002 [0x411fd080]
[ 0.155255] Detected PIPT I-cache on CPU3
[ 0.155297] GICv3: CPU3: found redistributor 3 region 0:0x0000000001960000
[ 0.155310] GICv3: CPU3: using allocated LPI pending table @0x0000000920090000
[ 0.155332] CPU3: Booted secondary processor 0x0000000003 [0x411fd080]
[ 0.169290] Detected PIPT I-cache on CPU4
[ 0.169367] GICv3: CPU4: found redistributor 100 region 0:0x0000000001980000
[ 0.169381] GICv3: CPU4: using allocated LPI pending table @0x00000009200a0000
[ 0.169413] CPU4: Booted secondary processor 0x0000000100 [0x411fd080]
[ 0.183379] Detected PIPT I-cache on CPU5
[ 0.183429] GICv3: CPU5: found redistributor 101 region 0:0x00000000019a0000
[ 0.183441] GICv3: CPU5: using allocated LPI pending table @0x00000009200b0000
[ 0.183464] CPU5: Booted secondary processor 0x0000000101 [0x411fd080]
[ 0.197401] Detected PIPT I-cache on CPU6
[ 0.197452] GICv3: CPU6: found redistributor 102 region 0:0x00000000019c0000
[ 0.197465] GICv3: CPU6: using allocated LPI pending table @0x00000009200c0000
[ 0.197488] CPU6: Booted secondary processor 0x0000000102 [0x411fd080]
[ 0.211418] Detected PIPT I-cache on CPU7
[ 0.211470] GICv3: CPU7: found redistributor 103 region 0:0x00000000019e0000
[ 0.211482] GICv3: CPU7: using allocated LPI pending table @0x00000009200d0000
[ 0.211506] CPU7: Booted secondary processor 0x0000000103 [0x411fd080]
[ 0.211551] smp: Brought up 1 node, 8 CPUs
[ 0.392534] SMP: Total of 8 processors activated.
[ 0.397340] CPU features: detected: 32-bit EL0 Support
[ 0.402596] CPU features: detected: CRC32 instructions
[ 0.407886] CPU: All CPU(s) started at EL2
[ 0.412075] alternatives: applying system-wide alternatives
[ 0.418741] devtmpfs: initialized
[ 0.431792] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.441769] futex hash table entries: 2048 (order: 5, 131072 bytes, linear)
[ 0.470983] pinctrl core: initialized pinctrl subsystem
[ 0.476646] DMI not present or invalid.
[ 0.480897] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.488207] DMA: preallocated 4096 KiB GFP_KERNEL pool for atomic allocations
[ 0.496218] DMA: preallocated 4096 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.504931] DMA: preallocated 4096 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.513159] audit: initializing netlink subsys (disabled)
[ 0.518774] audit: type=2000 audit(0.380:1): state=initialized audit_enabled=0 res=1
[ 0.518980] thermal_sys: Registered thermal governor 'step_wise'
[ 0.526693] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.532913] cpuidle: using governor menu
[ 0.543649] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.550672] ASID allocator initialised with 65536 entries
[ 0.564931] platform a000000.dp-bridge: Fixed dependency cycle(s) with /dp0-connector
[ 0.573376] KASLR disabled due to lack of seed
[ 0.580912] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.587860] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.594265] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.601200] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.607603] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.614537] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.620939] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.627874] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.635100] k3-chipinfo 43000014.chipid: Family:J784S4 rev:SR1.0 JTAGID[0x0bb8002f] Detected
[ 0.644451] iommu: Default domain type: Translated
[ 0.649468] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.655992] SCSI subsystem initialized
[ 0.659981] usbcore: registered new interface driver usbfs
[ 0.665599] usbcore: registered new interface driver hub
[ 0.671038] usbcore: registered new device driver usb
[ 0.676411] pps_core: LinuxPPS API ver. 1 registered
[ 0.681483] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.690822] PTP clock support registered
[ 0.694896] EDAC MC: Ver: 3.0.0
[ 0.698572] FPGA manager framework
[ 0.702082] Advanced Linux Sound Architecture Driver Initialized.
[ 0.708696] clocksource: Switched to clocksource arch_sys_counter
[ 0.715037] VFS: Disk quotas dquot_6.6.0
[ 0.719064] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.729036] Carveout Heap: Exported 512 MiB at 0x0000000900000000
[ 0.735314] NET: Registered PF_INET protocol family
[ 0.740640] IP idents hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.753362] tcp_listen_portaddr_hash hash table entries: 16384 (order: 6, 262144 bytes, linear)
[ 0.762393] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.770324] TCP established hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.779410] TCP bind hash table entries: 65536 (order: 9, 2097152 bytes, linear)
[ 0.787805] TCP: Hash tables configured (established 262144 bind 65536)
[ 0.794675] UDP hash table entries: 16384 (order: 7, 524288 bytes, linear)
[ 0.802031] UDP-Lite hash table entries: 16384 (order: 7, 524288 bytes, linear)
[ 0.809911] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.815971] RPC: Registered named UNIX socket transport module.
[ 0.822029] RPC: Registered udp transport module.
[ 0.826831] RPC: Registered tcp transport module.
[ 0.831634] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.838218] NET: Registered PF_XDP protocol family
[ 0.843119] PCI: CLS 0 bytes, default 64
[ 0.847807] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ 0.856975] Initialise system trusted keyrings
[ 0.861625] workingset: timestamp_bits=46 max_order=23 bucket_order=0
[ 0.870724] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.876957] NFS: Registering the id_resolver key type
[ 0.882149] Key type id_resolver registered
[ 0.886421] Key type id_legacy registered
[ 0.890544] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.897393] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.905013] 9p: Installing v9fs 9p2000 file system support
[ 0.930135] Key type asymmetric registered
[ 0.934318] Asymmetric key parser 'x509' registered
[ 0.939323] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.946948] io scheduler mq-deadline registered
[ 0.951579] io scheduler kyber registered
[ 0.957674] pinctrl-single 4301c000.pinctrl: 13 pins, size 52
[ 0.963637] pinctrl-single 4301c038.pinctrl: 11 pins, size 44
[ 0.969622] pinctrl-single 4301c068.pinctrl: 72 pins, size 288
[ 0.975645] pinctrl-single 4301c190.pinctrl: 1 pins, size 4
[ 0.981463] pinctrl-single 11c000.pinctrl: 72 pins, size 288
[ 0.987677] pinctrl-single a40000.pinctrl: 512 pins, size 2048
[ 0.997570] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.008474] loop: module loaded
[ 1.012372] megasas: 07.719.03.00-rc1
[ 1.018027] tun: Universal TUN/TAP device driver, 1.6
[ 1.023483] thunder_xcv, ver 1.0
[ 1.026793] thunder_bgx, ver 1.0
[ 1.030146] nicpf, ver 1.0
[ 1.033144] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.040526] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.045973] hclge is initializing
[ 1.049366] e1000: Intel(R) PRO/1000 Network Driver
[ 1.054348] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.060233] e1000e: Intel(R) PRO/1000 Network Driver
[ 1.065306] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.071366] igb: Intel(R) Gigabit Ethernet Network Driver
[ 1.076881] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.082583] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.088986] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.095094] sky2: driver version 1.30
[ 1.099205] VFIO - User Level meta-driver version: 0.3
[ 1.104750] usbcore: registered new interface driver usb-storage
[ 1.111278] i2c_dev: i2c /dev entries driver
[ 1.116545] sdhci: Secure Digital Host Controller Interface driver
[ 1.122862] sdhci: Copyright(c) Pierre Ossman
[ 1.127551] Synopsys Designware Multimedia Card Interface Driver
[ 1.133932] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.140245] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.146471] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.153185] usbcore: registered new interface driver usbhid
[ 1.158878] usbhid: USB HID core driver
[ 1.163477] optee: probing for conduit method.
I/TC: Reserved shared memory is enabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
[ 1.168032] optee: revision 3.20 (8e74d476)
[ 1.184437] optee: dynamic shared memory is enabled
[ 1.193909] optee: initialized driver
[ 1.198587] Initializing XFRM netlink socket
[ 1.202968] NET: Registered PF_PACKET protocol family
[ 1.208196] 9pnet: Installing 9P2000 support
[ 1.212583] Key type dns_resolver registered
[ 1.217123] registered taskstats version 1
[ 1.221320] Loading compiled-in X.509 certificates
[ 1.231629] ti-sci 44083000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)')
[ 1.263653] omap_i2c 42120000.i2c: bus 1 rev0.12 at 400 kHz
[ 1.269934] pca953x 0-0020: supply vcc not found, using dummy regulator
[ 1.276749] pca953x 0-0020: using no AI
[ 1.293329] pca953x 0-0022: supply vcc not found, using dummy regulator
[ 1.300127] pca953x 0-0022: using AI
[ 1.304441] omap_i2c 2000000.i2c: bus 0 rev0.12 at 400 kHz
[ 1.310248] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 177 domain created
[ 1.318790] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 10 domain created
[ 1.328039] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 283 domain created
[ 1.336712] ti-sci-inta 33d00000.msi-controller: Interrupt Aggregator domain 321 created
[ 1.348662] ti-udma 311a0000.dma-controller: Number of rings: 48
[ 1.355434] ti-udma 311a0000.dma-controller: Channels: 24 (bchan: 0, tchan: 8, rchan: 16)
[ 1.364613] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:328
[ 1.374489] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[ 1.381249] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[ 1.390077] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[878,128] sci-dev-id:315
[ 1.400224] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[ 1.406984] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[ 1.414892] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 214, base_baud = 6000000) is a 8250
[ 1.424313] 2880000.serial: ttyS2 at MMIO 0x2880000 (irq = 215, base_baud = 3000000) is a 8250
[ 1.433169] printk: console [ttyS2] enabled
[ 1.433169] printk: console [ttyS2] enabled
[ 1.441611] printk: bootconsole [ns16550a0] disabled
[ 1.441611] printk: bootconsole [ns16550a0] disabled
[ 1.492701] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.501526] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 1.509795] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Po0
[ 1.522642] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 1.529849] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 1.535998] pps pps0: new PPS source ptp0
[ 1.540141] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[ 1.588704] davinci_mdio c200f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.597305] davinci_mdio c200f00.mdio: phy[0]: device c200f00.mdio:00, driver TI DP83867
[ 1.605398] am65-cpsw-nuss c200000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Por0
[ 1.618130] am65-cpsw-nuss c200000.ethernet: Use random MAC address
[ 1.624388] am65-cpsw-nuss c200000.ethernet: initialized cpsw ale version 1.4
[ 1.631508] am65-cpsw-nuss c200000.ethernet: ALE Table size 64
[ 1.637623] am65-cpsw-nuss c200000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[ 1.647807] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010c, freq:250000000, add_val:3 pps:0
[ 1.757760] mmc0: CQHCI version 5.10
[ 1.802259] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[ 1.897169] mmc0: Command Queue Engine enabled
[ 1.901610] mmc0: new HS400 MMC card at address 0001
[ 1.906904] mmcblk0: mmc0:0001 G1M15L 29.6 GiB
[ 1.913746] mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 p16 p17
[ 1.922115] mmcblk0boot0: mmc0:0001 G1M15L 31.5 MiB
[ 1.927729] mmcblk0boot1: mmc0:0001 G1M15L 31.5 MiB
[ 1.933231] mmcblk0rpmb: mmc0:0001 G1M15L 4.00 MiB, chardev (240:0)
[ 1.956953] tps6594-rtc tps6594-rtc.4.auto: registered as rtc0
[ 1.963689] tps6594-rtc tps6594-rtc.4.auto: setting system clock to 2022-04-28T20:09:32 UTC (1651176572)
[ 1.973498] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fca100
[ 1.980293] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fca100
[ 1.987084] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fca100
[ 1.993877] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fca100
[ 2.000675] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fca100
[ 2.007461] omap-mailbox 31f85000.mailbox: omap mailbox rev 0x66fca100
[ 2.015933] ti-udma 285c0000.dma-controller: Channels: 22 (tchan: 11, rchan: 11, gp-rflow: 8)
[ 2.025911] ti-udma 31150000.dma-controller: Channels: 66 (tchan: 33, rchan: 33, gp-rflow: 16)
[ 2.038034] spi-nor spi0.0: unrecognized JEDEC id bytes: ff ef dc 21 00 00
[ 2.047171] spi-nor spi1.0: mt25qu512a (65536 Kbytes)
[ 2.052259] 7 fixed-partitions partitions found on MTD device 47050000.spi.0
[ 2.059296] Creating 7 MTD partitions on "47050000.spi.0":
[ 2.064767] 0x000000000000-0x000000080000 : "qspi.tiboot3"
[ 2.070896] 0x000000080000-0x000000280000 : "qspi.tispl"
[ 2.076753] 0x000000280000-0x000000680000 : "qspi.u-boot"
[ 2.082692] 0x000000680000-0x0000006c0000 : "qspi.env"
[ 2.088359] 0x0000006c0000-0x000000700000 : "qspi.env.backup"
[ 2.094615] 0x000000800000-0x000003fc0000 : "qspi.rootfs"
[ 2.100538] 0x000003fc0000-0x000004000000 : "qspi.phypattern"
[ 2.144705] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 2.153521] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 2.161789] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Po0
[ 2.174647] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 2.181870] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 2.188005] pps pps0: new PPS source ptp1
[ 2.192151] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[ 2.202178] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[ 2.248705] davinci_mdio c200f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 2.257421] davinci_mdio c200f00.mdio: phy[0]: device c200f00.mdio:00, driver TI DP83867
[ 2.265512] am65-cpsw-nuss c200000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Por0
[ 2.278255] am65-cpsw-nuss c200000.ethernet: Use random MAC address
[ 2.284511] am65-cpsw-nuss c200000.ethernet: initialized cpsw ale version 1.4
[ 2.291629] am65-cpsw-nuss c200000.ethernet: ALE Table size 64
[ 2.297773] am65-cpsw-nuss c200000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[ 2.307708] am65-cpsw-nuss c200000.ethernet: set new flow-id-base 82
[ 2.315512] debugfs: Directory 'pd:74' with parent 'pm_genpd' already present!
[ 2.322756] debugfs: Directory 'pd:73' with parent 'pm_genpd' already present!
[ 2.330039] debugfs: Directory 'pd:72' with parent 'pm_genpd' already present!
[ 2.330118] mmc1: CQHCI version 5.10
[ 2.337752] debugfs: Directory 'pd:335' with parent 'pm_genpd' already present!
[ 2.348134] debugfs: Directory 'pd:333' with parent 'pm_genpd' already present!
[ 2.355446] debugfs: Directory 'pd:332' with parent 'pm_genpd' already present!
[ 2.369348] ALSA device list:
[ 2.372308] No soundcards found.
[ 2.381698] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[ 2.389280] Waiting for root device PARTUUID=9bc8b883-02...
[ 2.449602] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 2.456573] mmcblk1: mmc1:aaaa SL32G 29.7 GiB
[ 2.465419] mmcblk1: p1 p2
[ 2.489535] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
[ 2.498073] VFS: Mounted root (ext4 filesystem) on device 179:98.
[ 2.509958] devtmpfs: mounted
[ 2.513724] Freeing unused kernel memory: 2176K
[ 2.518353] Run /sbin/init as init process
[ 2.717972] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRY)
[ 2.749416] systemd[1]: Detected architecture arm64.
Welcome to Arago 2023.04!
[ 2.823429] systemd[1]: Hostname set to <j784s4-evm>.
[ 2.887089] systemd-sysv-generator[188]: SysV service '/etc/init.d/umountnfs.sh' lacks a native systemd unit file. Autom.
[ 2.913185] systemd-sysv-generator[188]: SysV service '/etc/init.d/sysrepo' lacks a native systemd unit file. Automatica.
[ 2.936994] systemd-sysv-generator[188]: SysV service '/etc/init.d/inetd.busybox' lacks a native systemd unit file. Auto.
[ 2.961883] systemd-sysv-generator[188]: SysV service '/etc/init.d/psplash.sh' lacks a native systemd unit file. Automat.
[ 2.985880] systemd-sysv-generator[188]: SysV service '/etc/init.d/save-rtc.sh' lacks a native systemd unit file. Automa.
[ 3.009994] systemd-sysv-generator[188]: SysV service '/etc/init.d/netopeer2-server' lacks a native systemd unit file. A.
[ 3.034523] systemd-sysv-generator[188]: SysV service '/etc/init.d/telnetd' lacks a native systemd unit file. Automatica.
[ 3.058436] systemd-sysv-generator[188]: SysV service '/etc/init.d/dropbear' lacks a native systemd unit file. Automatic.
[ 3.082436] systemd-sysv-generator[188]: SysV service '/etc/init.d/single' lacks a native systemd unit file. Automatical.
[ 3.106243] systemd-sysv-generator[188]: SysV service '/etc/init.d/reboot' lacks a native systemd unit file. Automatical.
[ 3.129895] systemd-sysv-generator[188]: SysV service '/etc/init.d/autolaunch-demo' lacks a native systemd unit file. Au.
[ 3.154610] systemd-sysv-generator[188]: SysV service '/etc/init.d/halt' lacks a native systemd unit file. Automatically.
[ 3.178176] systemd-sysv-generator[188]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. .
[ 3.204078] systemd-sysv-generator[188]: SysV service '/etc/init.d/umountfs' lacks a native systemd unit file. Automatic.
[ 3.227972] systemd-sysv-generator[188]: SysV service '/etc/init.d/docker.init' lacks a native systemd unit file. Automa.
[ 3.252739] systemd-sysv-generator[188]: SysV service '/etc/init.d/netperf' lacks a native systemd unit file. Automatica.
[ 3.276992] systemd-sysv-generator[188]: SysV service '/etc/init.d/sendsigs' lacks a native systemd unit file. Automatic.
[ 3.406608] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
[ 3.415508] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
[ 3.441673] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically .
[ 3.486954] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatical.
[ 3.536238] systemd[1]: Queued start job for default target Graphical Interface.
[ 3.579803] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty.
[ 3.602010] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 3.625767] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 3.649582] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 3.672852] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ 3.696797] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 3.720874] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 3.736761] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 3.756741] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 3.772755] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 3.815166] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 3.840816] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 3.865655] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 3.888871] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 3.913006] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 3.932907] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 3.952933] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 3.968971] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 3.992979] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 4.012863] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 4.032893] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 4.068948] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 4.086983] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 4.110976] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 4.128920] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/s.
[ 4.160931] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 4.176989] systemd[1]: Create List of Static Device Nodes was skipped because of a failed condition check (ConditionFil.
[ 4.194504] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 4.210796] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 4.226849] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 4.249684] systemd[1]: Starting Start psplash boot splash screen...
Starting Start psplash boot splash screen...
[ 4.278020] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 4.292870] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathI.
[ 4.308557] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 4.333663] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 4.351431] systemd[1]: Starting Generate network units from Kernel command line...
Starting Generate network …ts from Kernel command line...
[ 4.379520] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems 4.391722] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
[0m...
[ 4.411486] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 4.432940] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 4.449049] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory /tmp.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star…progress communication helper.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Finished Generate network units from Kernel command line.
[ OK ] Finished Remount Root and Kernel File Systems.
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 4.751857] systemd-journald[205]: Received client request to flush runtime journal.
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Preparation for Local File Systems.
Mounting /media/ram...
Mounting /var/volatile...
[ 4.943071] audit: type=1334 audit(1651176575.476:2): prog-id=5 op=LOAD
[ 4.949700] audit: type=1334 audit(1651176575.484:3): prog-id=6 op=LOAD
Starting Rule-based Manage…for Device Events and Files...
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
[ OK ] Started Rule-based Manager for Device Events and Files.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Found device /dev/ttyS2.
[ OK ] Finished Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timer Units.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API...
[ OK ] Listening on dropbear.socket.
Starting Weston socket...
Starting Console System Startup Logging...
Starting D-Bus System Message Bus...
Starting Reboot and dump vmcore via kexec...
[ OK ] Listening on Docker Socket for the API.
[ OK ] Listening on Weston socket.
[ OK ] Finished Console System Startup Logging.
[ OK ] Finished Reboot and dump vmcore via kexec.
[ OK ] Reached target Socket Units.
[ 5.792705] random: crng init done
[ OK ] Finished Load/Save Random Seed.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting Telephony service...
Starting Expand the rootfs…ll size of the boot device....
[ OK ] Started startwlanap.[ 5.988345] audit: type=1334 audit(1651176576.520:4): prog-id=7 op=LOAD
[ OK ] Started startwlansta.
[ 6.004924] audit: type=1334 audit(1651176576.532:5): prog-id=8 op=LOAD
Starting User Login Management...
[ OK ] Started TEE Supplicant.
Starting telnetd.service...
[ OK ] Finished IPv6 Packet Filtering Framework.
[ OK ] Finished IPv4 Packet Filtering Framework.
[ OK ] Reached target Preparation for Network.
Starting Network Configuration...
[ OK ] Started telnetd.service.
[ OK ] Started Telephony service.
[ OK ] Started User Login Management.
[ OK ] Finished Expand the rootfs…full size of the boot device..
[ OK ] Started Network Configuration.
[ 6.340439] am65-cpsw-nuss c200000.ethernet eth1: PHY [c200f00.mdio:00] driver [TI DP83867] (irq=POLL)
[ 6.349868] am65-cpsw-nuss c200000.ethernet eth1: configuring for phy/rgmii-rxid link mode
Starting Wait for Network to be Configured...
Starting Network Name Resolution...
[ 6.373213] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[ 6.383034] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
Starting Avahi mDNS/DNS-SD Stack...
Starting Enable and configure wl18xx bluetooth stack...
Starting containerd container runtime...
[ OK ] Started Netperf Benchmark Server.
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Permit User Sessions...
[ OK ] Finished Enable and configure wl18xx bluetooth stack.
[ OK ] Finished Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
Starting Weston, a Wayland…ositor, as a system service...
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Created slice Slice /system/systemd-fsck.
[ OK ] Found device /dev/mmcblk1p1.
Starting File System Check on /dev/mmcblk1p1 6.794533] audit: type=1334 audit(1651176577.328:6): prog-id=9 op=LD
0m...
[ 6.803020] audit: type=1334 audit(1651176577.336:7): prog-id=10 op=LOAD
Starting User Database Manager...
[ OK ] Started User Database Manager.
[ OK ] Created slice User Slice of UID 1000.
Starting File System Check on /dev/mmcblk0p10...
Starting File System Check on /dev/mmcblk0p13...
Starting User Runtime Directory /run/user/1000...
[ OK ] Finished User Runtime Directory /run/user/1000.
[ OK ] Found device /dev/mmcblk0p8.
[ OK ] Finished File System Check on /dev/mmcblk1p1.
[ OK ] Finished File System Check on /dev/mmcblk0p10.
[ OK ] Finished File System Check on /dev/mmcblk0p13.
Mounting /run/media/BOOT-mmcblk1p1...
Mounting /run/media/linux-mmcblk0p10...
Mounting /run/media/linux-mmcblk0p13...
Starting File System Check on /dev/mmcblk0p11...
Starting File System Check on /dev/mmcblk0p12...
Starting File System Check on [ 7.220810] EXT4-fs (mmcblk0p10): mounted filesystem with ordered data mode. Quot.
/dev/mmcblk0p14...
Starting File System Check on /dev/mmcblk0p15...
Starting File [ 7.238391] EXT4-fs (mmcblk0p13): mounted filesystem with ordered data mode. Quota mode: none.
System Check on /dev/mmcblk0p16...
Starting File System Check on /dev/mmcblk0p17...
Starting File System Check on /dev/mmcblk0p8...
Starting User Manager for UID 1000...
[ OK ] Mounted /run/media/linux-mmcblk0p10.
[ 7.274455] audit: type=1006 audit(1651176577.808:8): pid=1276 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=421
32m OK ] Mounted /run/media/linux-mmcblk0p13.[ 7.291915] audit: type=1300 audit(1651176577.808:8): arch=c00000b7 sysca)
[ OK ] Finished File System Check on /de[ 7.323956] audit: type=1327 audit(1651176577.808:8): proctitle="(systemd)"
v/mmcblk0p11.
[ OK ] Found device /dev/mmcblk0p9.
Mounting /run/media/linux-mmcblk0p11...
Starting File System Check on /dev/mmcblk0p9...
[ OK ] Mounted /run/media/BOOT-mmcblk1p1.
[ OK ] Finished 7.361269] mmc0: running CQE recovery
39mFile System Check on /dev/mmcblk0p12.
[ OK [ 7.372074] mmc0: mmc_hs400_to_hs200 failed, error -84
] Finished File System Check on /dev/mmcblk0p15.
[ 7.378881] I/O error, dev mmcblk0, sector 21485602 op 0x0:(READ) flags 0x80700 phys_seg 1 prio class 2
Mounting /run/media/linux-mmcblk0p12...
[ 7.393769] mmc0: running CQE recovery
Mounting /run/media/linux-mmcblk0p15...
[ 7.403195] mmc0: running CQE recovery
0;32m OK ] Finished File System Check on /dev/mmc[ 7.412357] mmc0: running CQE recovery
blk0p14.
[ OK ] Finished File System [ 7.421648] mmc0: running CQE recovery
Check on /dev/mmcblk0p16.
Mounting /run/m[ 7.430927] mmc0: running CQE recovery
edia/linux-mmcblk0p14...
Mounting /run/me[ 7.440523] mmc0: cache flush error -84
dia/linux-mmcblk0p16...
[ OK ] Finished Synchronize System and HW clocks.
[ 7.531598] EXT4-fs (mmcblk0p11): mounted filesystem with ordered data mode. Quota mode: none.
[ 7.536302] EXT4-fs (mmcblk0p12): mounted filesystem with ordered data mode. Quota mode: none.
[ OK ] Mounted /run/media/linux-mmcblk0p11.
[ OK ] Finished File System Check on /dev/mmcblk0p17.
[ OK ] Finished File System Check on /dev/mmcblk0p8.
[ OK ] Mounted /run/media/linux-mmcblk0p12.
Mounting /run/media/linux-mmcblk0p17...
Mounting /run/media/linux-mmcblk0p8...
[ 7.614840] EXT4-fs (mmcblk0p14): mounted filesystem with ordered data mode. Quota mode: none.
[ 7.616780] EXT4-fs (mmcblk0p15): mounted filesystem with ordered data mode. Quota mode: none.
[ 7.631771] EXT4-fs (mmcblk0p16): mounted filesystem with ordered data mode. Quota mode: none.
[ OK ] Mounted /run/media/linux-mmcblk0p14.
[ OK ] Finished File System Check on /dev/mmcblk0p9.
[ OK ] Mounted /run[ 7.653875] EXT4-fs (mmcblk0p17): mounted filesystem with ordered data mode. Quota mode: none.
/media/linux-mmcblk0p15.
[ OK ] Mounted 7.654279] EXT4-fs (mmcblk0p8): mounted filesystem with ordered data mode. Quota mode: none.
39m/run/media/linux-mmcblk0p16.
[ OK ] Mounted /run/media/linux-mmcblk0p17.
[ OK ] Mounted /run/media/linux-mmcblk0p8.
[ OK ] Started User Manager for UID 1000.
[ OK ] Started Session c1 of User wes[ 7.896856] audit: type=1006 audit(1651176578.432:9): pid=1040 uid=0 old-auid=4291
ton.
[ 7.914637] audit: type=1300 audit(1651176578.432:9): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffc0fee088 a)
[ 7.941753] audit: type=1327 audit(1651176578.432:9): proctitle="(weston)"
[ OK ] Started containerd container runtime.
Mounting /run/media/linux-mmcblk0p9...
[ 8.094503] EXT4-fs (mmcblk0p9): mounted filesystem with ordered data mode. Quota mode: none.
[ OK ] Mounted /run/media/linux-mmcblk0p9.
[FAILED] Failed to start Weston, a …mpositor, as a system service.
See 'systemctl status weston.service' for details.
[DEPEND] Dependency failed for DEMO.
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPL-3.0 packages:
adwaita-icon-theme-symbolic
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
g++-symlinks
g++
gawk-dev
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gnu-config
grub-common
grub-editenv
grub-efi
gzip
less
libasm1
libatomic-dev
libatomic1
libbfd
libdebuginfod1
libdw1
libeigen-dev
libelf1
libgcc-s-dev
libgcc1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp10
libidn2-0
libmpc3
libmpfr6
libopcodes
libqt5charts-examples
libqt5charts-plugins
libqt5charts-qmlplugins
libqt5charts5
libqt5sensors-plugins
libqt5sensors-qmlplugins
libqt5sensors5
libqt5serialport-examples
libqt5serialport-plugins
libqt5serialport-qmlplugins
libqt5serialport5
libqt5svg-examples
libqt5svg-plugins
libqt5svg-qmlplugins
libqt5svg5
libqt5virtualkeyboard-plugins
libqt5virtualkeyboard-qmlplugins
libqt5virtualkeyboard5
libqt5webchannel-plugins
libqt5webchannel-qmlplugins
libqt5webchannel5
libreadline-dev
libreadline8
libstdc++-dev
libstdc++6
libunistring2
m4-dev
m4
make
nettle
parted
piglit
qt3d-plugins
qt3d-qmlplugins
qt3d
qtbase-examples
qtbase-plugins
qtbase-qmlplugins
qtbase
qtconnectivity-plugins
qtconnectivity-qmlplugins
qtconnectivity
qtdeclarative-plugins
qtdeclarative-qmlplugins
qtdeclarative-tools
qtdeclarative
qtgraphicaleffects-qmlplugins
qtlocation-examples
qtlocation-plugins
qtlocation-qmlplugins
qtlocation
qtmultimedia-examples
qtmultimedia-plugins
qtmultimedia-qmlplugins
qtmultimedia
qtquics-qmlplugins.control
qtquics2-plugins.control
qtquics2-qmlplugins.control
qtquics2.control
qtscript-examples
qtscript-plugins
qtscript-qmlplugins
qtscript
qtwayland-examples
qtwayland-plugins
qtwayland-qmlplugins
qtwayland
tar
which
If you do not wish to distribute GPL-3.0 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Finished Print notice about GPLv3 packages.
[ 10.438177] am65-cpsw-nuss c200000.ethernet eth1: Link is Up - 1Gbps/Full - flow control rx/tx
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project j784s4-evm -
Arago 2023.04 j784s4-evm -
j784s4-evm login: [ 12.452829] platform regulator-dp0-prw: deferred probe pending
[ 12.458665] platform regulator-dp1-prw: deferred probe pending
j784s4-evm login: root
[ 19.358336] audit: type=1006 audit(1651176589.892:10): pid=1696 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=42941
[ 19.370787] audit: type=1300 audit(1651176589.892:10): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffc0fee088 )
[ 19.397166] audit: type=1327 audit(1651176589.892:10): proctitle="(systemd)"
[ 19.404223] audit: type=1334 audit(1651176589.904:11): prog-id=11 op=LOAD
[ 19.411013] audit: type=1300 audit(1651176589.904:11): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffdbc6bd00)
[ 19.436432] audit: type=1327 audit(1651176589.904:11): proctitle="(systemd)"
[ 19.443482] audit: type=1334 audit(1651176589.904:12): prog-id=11 op=UNLOAD
[ 19.450443] audit: type=1334 audit(1651176589.904:13): prog-id=12 op=LOAD
[ 19.457232] audit: type=1300 audit(1651176589.904:13): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffdbc6bda0)
[ 19.482652] audit: type=1327 audit(1651176589.904:13): proctitle="(systemd)"
root@j784s4-evm:~# cat /sys/class/remoteproc/remoteproc*/name
cat: '/sys/class/remoteproc/remoteproc*/name': No such file or directory
ps:替换过自己编译的atf2.10-rc1