This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI!
We changed the AM6254 chip to AM6251,AM6251 is the fs-hs startup mode, only modified the CPU single-core configuration, the system can be started successfully, but in the kernel startup process will appear: A start job is running for udev wait for Complete Device Initialization (.. s / 3min), and it took a long time to continue to start, which is why? Where is the initialization problem?
The following is the log of the startup process:
U-Boot SPL 2021.01-00001-g45cb7e4-dirty (Nov 24 2023 - 13:11:00 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
SPL initial stack usage: 13424 bytes
Trying to boot from MMC2
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Authentication passed
Loading Environment from MMC... MMC Device 0 not found
*** Warning - No MMC card found, using default environment
Starting ATF on ARM64 core...
NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE: BL31: Built : 05:06:58, Feb 24 2023
U-Boot SPL 2021.01-00001-g45cb7e4-dirty (Nov 24 2023 - 13:15:54 +0800)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
Trying to boot from MMC2
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
U-Boot 2021.01-00001-g45cb7e4-dirty (Nov 24 2023 - 13:15:54 +0800)
SoC: AM62X SR1.0 HS-FS
Model: LICHAN-UBOOT Texas Instruments AM625 SK
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed 1
DRAM: 512 MiB
MMC: mmc@fa10000: 0, mmc@fa00000: 1, mmc@fa20000: 2
Loading Environment from MMC... *** Warning - No block device, using default environment
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed 1
Net: eth0: ethernet@8000000port@1
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
Failed to load 'uEnv.txt'
ERROR: reserving fdt memory region failed (addr=9e780000 size=80000)
ERROR: reserving fdt memory region failed (addr=9e800000 size=1800000)
ERROR: reserving fdt memory region failed (addr=9db00000 size=c00000)
1049772 bytes read in 67 ms (14.9 MiB/s)
ERROR: reserving fdt memory region failed (addr=9e780000 size=80000)
ERROR: reserving fdt memory region failed (addr=9e800000 size=1800000)
ERROR: reserving fdt memory region failed (addr=9db00000 size=c00000)
19542528 bytes read in 827 ms (22.5 MiB/s)
ERROR: reserving fdt memory region failed (addr=9e780000 size=80000)
ERROR: reserving fdt memory region failed (addr=9e800000 size=1800000)
ERROR: reserving fdt memory region failed (addr=9db00000 size=c00000)
51580 bytes read in 26 ms (1.9 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
ERROR: reserving fdt memory region failed (addr=9da00000 size=100000)
ERROR: reserving fdt memory region failed (addr=9db00000 size=c00000)
ERROR: reserving fdt memory region failed (addr=9e700000 size=80000)
ERROR: reserving fdt memory region failed (addr=9e780000 size=80000)
ERROR: reserving fdt memory region failed (addr=9e800000 size=1800000)
Loading Device Tree to 000000008fef0000, end 000000008fffffff ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.168-g2c23e6c538 (xuan@aaa) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Fri Nov 24 13:20:44 CST 2023
[ 0.000000] Machine model: LICHAN Texas Instruments AM625 SK
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000098800000, size 80 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x000000009fffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009d9fffff]
[ 0.000000] node 0: [mem 0x000000009da00000-0x000000009e6fffff]
[ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff]
[ 0.000000] node 0: [mem 0x000000009e780000-0x000000009fffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x000000009fffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 22 pages/cpu s51288 r8192 d30632 u90112
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129024
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=fa8c87b4-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 365404K/524288K available (11392K kernel code, 1164K rwdata, 4504K rodata, 1920K init, 433K bss, 76964K reserved, 81920K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=1.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 256 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000000080030000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080040000
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000005] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008509] Console: colour dummy device 80x25
[ 0.013103] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023785] pid_max: default: 32768 minimum: 301
[ 0.028583] LSM: Security Framework initializing
[ 0.033353] Mount-cache hash table entries: 1024 (order: 1, 8192 bytes, linear)
[ 0.040832] Mountpoint-cache hash table entries: 1024 (order: 1, 8192 bytes, linear)
[ 0.050427] rcu: Hierarchical SRCU implementation.
[ 0.055620] Platform MSI: msi-controller@1820000 domain created
[ 0.061919] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.071166] EFI services will not be available.
[ 0.075908] smp: Bringing up secondary CPUs ...
[ 0.080548] smp: Brought up 1 node, 1 CPU
[ 0.084647] SMP: Total of 1 processors activated.
[ 0.089463] CPU features: detected: 32-bit EL0 Support
[ 0.094719] CPU features: detected: CRC32 instructions
[ 0.107670] CPU: All CPU(s) started at EL2
[ 0.111876] alternatives: patching kernel code
[ 0.117405] devtmpfs: initialized
[ 0.127323] KASLR disabled due to lack of seed
[ 0.132101] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.142077] futex hash table entries: 256 (order: 2, 16384 bytes, linear)
[ 0.151534] pinctrl core: initialized pinctrl subsystem
[ 0.157607] DMI not present or invalid.
[ 0.162221] NET: Registered protocol family 16
[ 0.168217] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
[ 0.175533] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.183543] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.192212] thermal_sys: Registered thermal governor 'step_wise'
[ 0.192218] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.198745] cpuidle: using governor menu
[ 0.209641] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.216614] ASID allocator initialised with 65536 entries
[ 0.246122] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.253053] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.259973] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.266829] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.274725] cryptd: max_cpu_qlen set to 1000
[ 0.282056] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected
[ 0.291197] vcc_5v0: supplied by vmain_pd
[ 0.296036] vcc_3v3_sys: supplied by vmain_pd
[ 0.300878] vdd_mmc1: supplied by vcc_3v3_sys
[ 0.305623] wlan_lten: supplied by vcc_3v3_sys
[ 0.310424] wlan_en: supplied by wlan_lten
[ 0.314878] vcc_1v8: supplied by vcc_3v3_sys
[ 0.320457] iommu: Default domain type: Translated
[ 0.325796] SCSI subsystem initialized
[ 0.330120] mc: Linux media interface: v0.10
[ 0.334510] videodev: Linux video capture interface: v2.00
[ 0.340182] pps_core: LinuxPPS API ver. 1 registered
[ 0.345259] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.354608] PTP clock support registered
[ 0.358646] EDAC MC: Ver: 3.0.0
[ 0.362509] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100
[ 0.369661] FPGA manager framework
[ 0.373244] Advanced Linux Sound Architecture Driver Initialized.
[ 0.380363] clocksource: Switched to clocksource arch_sys_counter
[ 0.386866] VFS: Disk quotas dquot_6.6.0
[ 0.390932] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.402699] NET: Registered protocol family 2
[ 0.407352] IP idents hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.415544] tcp_listen_portaddr_hash hash table entries: 256 (order: 0, 4096 bytes, linear)
[ 0.424217] TCP established hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.432173] TCP bind hash table entries: 4096 (order: 4, 65536 bytes, linear)
[ 0.439546] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.446182] UDP hash table entries: 256 (order: 1, 8192 bytes, linear)
[ 0.452891] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes, linear)
[ 0.460139] NET: Registered protocol family 1
[ 0.464985] RPC: Registered named UNIX socket transport module.
[ 0.471075] RPC: Registered udp transport module.
[ 0.475885] RPC: Registered tcp transport module.
[ 0.480694] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.487284] NET: Registered protocol family 44
[ 0.491839] PCI: CLS 0 bytes, default 64
[ 0.496541] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.508749] Initialise system trusted keyrings
[ 0.513539] workingset: timestamp_bits=46 max_order=17 bucket_order=0
[ 0.524002] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.530652] NFS: Registering the id_resolver key type
[ 0.535909] Key type id_resolver registered
[ 0.540188] Key type id_legacy registered
[ 0.544339] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.551200] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.558782] ntfs: driver 2.1.32 [Flags: R/W DEBUG].
[ 0.564043] 9p: Installing v9fs 9p2000 file system support
[ 0.604267] Key type asymmetric registered
[ 0.608492] Asymmetric key parser 'x509' registered
[ 0.613557] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.621176] io scheduler mq-deadline registered
[ 0.625823] io scheduler kyber registered
[ 0.632014] pinctrl-single 4084000.pinctrl: 34 pins, size 136
[ 0.638399] pinctrl-single f4000.pinctrl: 171 pins, size 684
[ 0.651870] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.664622] panel-simple panel-rgb: supply power not found, using dummy regulator
[ 0.672473] panel-simple panel-rgb: Expected bpc in {6,8} but got: 0
[ 0.686019] brd: module loaded
[ 0.695147] loop: module loaded
[ 0.699300] megasas: 07.714.04.00-rc1
[ 0.706815] tun: Universal TUN/TAP device driver, 1.6
[ 0.712676] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 0.719101] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.725222] sky2: driver version 1.30
[ 0.729934] VFIO - User Level meta-driver version: 0.3
[ 0.736054] i2c /dev entries driver
[ 0.741484] sdhci: Secure Digital Host Controller Interface driver
[ 0.747871] sdhci: Copyright(c) Pierre Ossman
[ 0.752813] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.759670] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.766128] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.774306] optee: probing for conduit method.
[ 0.778949] optee: revision 3.20 (8e74d476)
[ 0.779215] optee: dynamic shared memory is enabled
[ 0.788727] optee: initialized driver
[ 0.794379] NET: Registered protocol family 17
[ 0.799174] 9pnet: Installing 9P2000 support
[ 0.803643] Key type dns_resolver registered
[ 0.808418] Loading compiled-in X.509 certificates
[ 0.825144] ti-sci 44043000.system-controller: lpm region is required for suspend but not provided.
[ 0.834546] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
[ 0.901186] omap-gpmc 3b000000.memory-controller: GPMC revision 6.0
[ 0.907659] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 0.915744] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0x48
[ 0.922274] nand: Micron MT29F16G08ABACAWP
[ 0.926464] nand: 2048 MiB, SLC, erase size: 512 KiB, page size: 4096, OOB size: 224
[ 0.934387] omap2-nand 51000000.nand: using prefetch polled xfer mode
[ 0.941045] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[ 0.946480] platform 25010000.ecc: Unable to configure elm - device not probed?
[ 0.955226] omap_i2c 4900000.i2c: bus 0 rev0.12 at 100 kHz
[ 0.961731] omap_i2c 2b200000.i2c: bus 1 rev0.12 at 100 kHz
[ 0.968602] omap_i2c 20010000.i2c: bus 2 rev0.12 at 100 kHz
[ 0.974803] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
[ 0.983237] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
[ 0.992623] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[ 1.003822] ti-udma 485c0100.dma-controller: Number of rings: 82
[ 1.012083] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
[ 1.023198] ti-udma 485c0000.dma-controller: Number of rings: 150
[ 1.033845] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
[ 1.044461] printk: console [ttyS2] disabled
[ 1.048957] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 29, base_baud = 3000000) is a 8250
[ 1.057738] printk: console [ttyS2] enabled
[ 1.057738] printk: console [ttyS2] enabled
[ 1.066182] printk: bootconsole [ns16550a0] disabled
[ 1.066182] printk: bootconsole [ns16550a0] disabled
[ 1.077129] omap8250 2830000.serial: failed to get alias
[ 1.083263] omap8250 2840000.serial: failed to get alias
[ 1.089196] omap8250 2850000.serial: failed to get alias
[ 1.095076] omap8250 2860000.serial: failed to get alias
[ 1.102755] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
[ 1.116677] Logo parameter width:1366 ,height:768
[ 1.116677]
[ 1.122071] clutsize: 224
[ 1.145357] Console: switching to colour frame buffer device 170x48
[ 1.178828] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device
[ 1.194378] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[ 1.240385] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.249637] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver unknown
[ 1.257577] davinci_mdio 8000f00.mdio: phy[2]: device 8000f00.mdio:02, driver unknown
[ 1.265536] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
[ 1.278568] am65-cpsw-nuss 8000000.ethernet: Use random MAC address
[ 1.284847] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
[ 1.291972] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[ 1.298667] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0
[ 1.309256] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[ 1.421878] mmc1: CQHCI version 5.10
[ 1.434576] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0x48
[ 1.441045] nand: Micron MT29F16G08ABACAWP
[ 1.445136] nand: 2048 MiB, SLC, erase size: 512 KiB, page size: 4096, OOB size: 224
[ 1.452887] omap2-nand 51000000.nand: using prefetch polled xfer mode
[ 1.459381] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[ 1.464806] 8 fixed-partitions partitions found on MTD device omap2-nand.0
[ 1.471675] Creating 8 MTD partitions on "omap2-nand.0":
[ 1.476992] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[ 1.484472] 0x000000000000-0x000000200000 : "NAND.tiboot3"
[ 1.491932] 0x000000200000-0x000000400000 : "NAND.tispl"
[ 1.498439] 0x000000400000-0x000000800000 : "NAND.u-boot"
[ 1.505284] 0x000000800000-0x000000840000 : "NAND.u-boot-env"
[ 1.511072] mtd: partition "NAND.u-boot-env" doesn't end on an erase/write block -- force read-only
[ 1.521451] 0x000000840000-0x0000008c0000 : "NAND.dtb"
[ 1.526619] mtd: partition "NAND.dtb" doesn't start on an erase/write block boundary -- force read-only
[ 1.536999] 0x0000008c0000-0x000000ac0000 : "NAND.logo"
[ 1.542258] mtd: partition "NAND.logo" doesn't start on an erase/write block boundary -- force read-only
[ 1.552800] 0x000000ac0000-0x0000023c0000 : "NAND.kernel"
[ 1.558259] mtd: partition "NAND.kernel" doesn't start on an erase/write block boundary -- force read-only
[ 1.571219] 0x0000023c0000-0x00001efc0000 : "NAND.file-system"
[ 1.577063] mtd: partition "NAND.file-system" doesn't start on an erase/write block boundary -- force read-only
[ 1.599823] mmc1: new high speed SDHC card at address aaaa
[ 1.612732] mmcblk1: mmc1:aaaa SC16G 14.8 GiB
[ 1.646263] debugfs: Directory 'pd:53' with parent 'pm_genpd' already present!
[ 1.653723] mmcblk1: p1 p2
[ 1.657563] debugfs: Directory 'pd:52' with parent 'pm_genpd' already present!
[ 1.664884] debugfs: Directory 'pd:51' with parent 'pm_genpd' already present!
[ 1.672485] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
[ 1.691499] ALSA device list:
[ 1.694528] No soundcards found.
[ 2.470930] EXT4-fs (mmcblk1p2): recovery complete
[ 2.476829] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.485000] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.494786] devtmpfs: mounted
[ 2.499206] Freeing unused kernel memory: 1920K
[ 2.503871] Run /sbin/init as init process
[ 2.801540] systemd[1]: System time before build time, advancing clock.
[ 2.882513] NET: Registered protocol family 10
[ 2.888024] Segment Routing with IPv6
[ 2.933260] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 2.955399] systemd[1]: Detected architecture arm64.
Welcome to Arago 2021.09!
[ 2.987452] systemd[1]: Set hostname to <am62xx-evm>.
[ 5.611172] systemd-sysv-generator[170]: Overwriting existing symlink /run/systemd/generator.late/sshd.service with real service.
[ 5.777969] systemd[1]: /lib/systemd/system/startwlansta.service:7: Unknown key name 'After' in section 'Service', ignoring.
[ 5.803756] systemd[1]: /lib/systemd/system/irqbalanced.service:6: Unknown key name 'ConditionCPUs' in section 'Unit', ignoring.
[ 5.835786] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock 鈫/run/docker.sock; please update the unit file accordingly.
[ 5.947270] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.958155] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 5.980569] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.989116] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 6.012543] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.020836] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 6.044884] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password 鈥s to Console Directory Watch.
[ 6.068673] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R鈥ests to Wall Directory Watch.
[ 6.092648] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 6.112514] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 6.132476] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 6.152475] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 6.192344] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 6.216698] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 6.243385] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 6.264922] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 6.291911] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 6.300919] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 6.325166] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 6.345270] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 6.369075] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 6.388898] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 6.413502] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 6.441532] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 6.477351] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 6.511907] systemd[1]: Mounting Temporary Directory (/tmp)...
Mounting Temporary Directory (/tmp)...
[ 6.545841] systemd[1]: Starting Create list of static device nodes for the current kernel...
Starting Create list of st鈥des for the current kernel...
[ 6.584779] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 6.597356] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 6.615544] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 6.652778] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 6.689647] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 6.716754] cryptodev: loading out-of-tree module taints kernel.
[ 6.733296] systemd[1]: Starting udev Coldplug all Devices...
Starting udev Coldplug all Devices...
[ 6.769158] cryptodev: driver 1.10 loaded.
[ 6.775436] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 6.805046] systemd[1]: Mounted Huge Pages File System.
[ OK ] Mounted Huge Pages File System.
[ 6.833636] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 6.863239] systemd[1]: Mounted Kernel Debug File System.
[ 6.874082] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[ OK ] Mounted Kernel Debug File System.
[ 6.897408] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Create list of sta鈥nodes for the current kernel.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Remount Root and Kernel File Systems.
[ 7.009900] random: systemd: uninitialized urandom read (16 bytes read)
[ 7.019268] random: systemd-journal: uninitialized urandom read (16 bytes read)
Mounting Kernel Configuration File System...
[ 7.049905] random: systemd-journal: uninitialized urandom read (16 bytes read)
Starting Flush Journal to Persistent Storage...
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev 7.123656] systemd-journald[182]: Received client request to flush runtime journal.
m...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started udev Coldplug all Devices.
Starting udev Wait for Complete Device Initialization...
[ OK ] Started Network Time Synchronization.
[ 8.225430] random: systemd: uninitialized urandom read (16 bytes read)
[ OK ] Reached target System Time Set.
[ 8.256788] random: systemd: uninitialized urandom read (16 bytes read)
[ OK ] Reached target System Time Synchronized.
[ 8.704178] random: systemd: uninitialized urandom read (16 bytes read)
[ 9.132521] rtc-ds1307 2-0068: registered as rtc0
[ 9.168414] random: crng init done
[ 9.171834] random: 61 urandom warning(s) missed due to ratelimiting
[ OK ] Started Load/Save Random Seed.
[ 9.221309] rtc-ds1307 2-0068: setting system clock to 2023-11-24T08:40:31 UTC (1700815231)
[ 10.452618] Internal error: synchronous external abort: 96000010 [#1] PREEMPT SMP
[ 10.460112] Modules linked in: rti_wdt(+) sa2ul j721e_csi2rx videobuf2_dma_contig sha512_generic authenc videobuf2_memops videobuf2_v4l2 mcrc videobuf2_common cdns_dphy pruss rtc_ds1307 sch_fq_codel cryptodev(O) ipv6
[ 10.479335] CPU: 0 PID: 209 Comm: systemd-udevd Tainted: G O 5.10.168-g2c23e6c538 #1
[ 10.488358] Hardware name: LICHAN Texas Instruments AM625 SK (DT)
[ 10.494437] pstate: 80000005 (Nzcv daif -PAN -UAO -TCO BTYPE=--)
[ 10.500440] pc : rti_wdt_probe+0x1e0/0x4e8 [rti_wdt]
[ 10.505392] lr : rti_wdt_probe+0x1d0/0x4e8 [rti_wdt]
[ 10.510342] sp : ffff8000116b3930
[ 10.513645] x29: ffff8000116b3930 x28: 0000000000000100
[ 10.518948] x27: ffff8000100f67a8 x26: 0000000000000003
[ 10.524248] x25: ffff800011254648 x24: 0000000000000038
[ 10.529547] x23: ffff0000042c8720 x22: ffff000000258000
[ 10.534847] x21: ffff0000042c8690 x20: ffff000000258010
[ 10.540147] x19: ffff0000042c8680 x18: 0000000000000000
[ 10.545447] x17: 0000000000000000 x16: 0000000000000000
[ 10.550746] x15: 00006e5e039fa8b6 x14: 000000000000024b
[ 10.556046] x13: 000000000000024b x12: ffff8000115b7000
[ 10.561346] x11: ffff8000115a7000 x10: 0000000000001000
[ 10.566645] x9 : ffff8000112a8000 x8 : ffff80001118a4a4
[ 10.571945] x7 : 0000000000000041 x6 : 000000000000008a
[ 10.577244] x5 : 000000000e011000 x4 : ffff000000258210
[ 10.582544] x3 : ffff000000252900 x2 : 0000000000000000
[ 10.587843] x1 : ffff00000427b900 x0 : ffff8000115a5090
[ 10.593144] Call trace:
[ 10.595584] rti_wdt_probe+0x1e0/0x4e8 [rti_wdt]
[ 10.600197] platform_drv_probe+0x54/0xa8
[ 10.604195] really_probe+0xec/0x400
[ 10.607759] driver_probe_device+0x58/0xb8
[ 10.611843] device_driver_attach+0x74/0x80
[ 10.616012] __driver_attach+0x68/0xf8
[ 10.619750] bus_for_each_dev+0x70/0xc0
[ 10.623573] driver_attach+0x24/0x30
[ 10.627137] bus_add_driver+0x150/0x200
[ 10.630961] driver_register+0x64/0x120
[ 10.634785] __platform_driver_register+0x48/0x58
[ 10.639477] rti_wdt_driver_init+0x24/0x1000 [rti_wdt]
[ 10.644607] do_one_initcall+0x54/0x1b8
[ 10.648432] do_init_module+0x44/0x1f0
[ 10.652171] load_module+0x1fbc/0x25d0
[ 10.655908] __do_sys_finit_module+0xb8/0xf8
[ 10.660164] __arm64_sys_finit_module+0x20/0x30
[ 10.664687] el0_svc_common.constprop.0+0x78/0x1c8
[ 10.669467] do_el0_svc+0x24/0xa0
[ 10.672773] el0_svc+0x14/0x20
[ 10.675817] el0_sync_handler+0xb0/0xb8
[ 10.679640] el0_sync+0x180/0x1c0
[ 10.682950] Code: f9000260 b140041f 54001128 91024000 (b9400000)
[ 10.689031] ---[ end trace 1d5ad7780324d2d0 ]---
[ 10.744440] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[ 10.805593] platform 78000000.r5f: configured R5F for IPC-only mode
[ 10.835583] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9da00000
[ 10.868949] remoteproc remoteproc0: 78000000.r5f is available
[ 10.920631] remoteproc remoteproc0: attaching to 78000000.r5f
[ 10.959708] platform 78000000.r5f: R5F core initialized in IPC-only mode
[ 11.000224] remoteproc0#vdev0buffer: assigned reserved memory node r5f-dma-memory@9da00000
[ 11.017679] PVR_K: 207: Read BVNC 33.15.11.3 from HW device registers
[ 11.050014] PVR_K: 207: RGX Device registered with BVNC 33.15.11.3
[ 11.078266] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 11.083853] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[ 11.096762] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[ 11.124105] [drm] Initialized pvr 1.15.6133109 20170530 for fd00000.gpu on minor 1
[ 11.139677] remoteproc0#vdev0buffer: registered virtio0 (type 7)
[ 11.170070] remoteproc remoteproc0: remote processor 78000000.r5f is now attached
[ 13.818785] remoteproc remoteproc1: 30074000.pru is available
[ 13.854051] remoteproc remoteproc2: 30078000.pru is available
[ 13.958730] cdns-csi2rx: probe of 30101000.csi-bridge failed with error -22
[ 14.135039] usbcore: registered new interface driver usbfs
[ 14.141674] usbcore: registered new interface driver hub
[ 14.148860] usbcore: registered new device driver usb
[ 14.179820] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 14.185535] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 14.195147] xhci-hcd xhci-hcd.0.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000000000010010
[ 14.205335] xhci-hcd xhci-hcd.0.auto: irq 492, io mem 0x31000000
[ 14.212123] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 14.218332] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 14.226571] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[ 14.233868] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 14.242438] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 14.249840] usb usb1: Product: xHCI Host Controller
[ 14.254863] usb usb1: Manufacturer: Linux 5.10.168-g2c23e6c538 xhci-hcd
[ 14.261614] usb usb1: SerialNumber: xhci-hcd.0.auto
[ 14.268575] hub 1-0:1.0: USB hub found
[ 14.273451] hub 1-0:1.0: 1 port detected
[ 14.280190] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 14.289866] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10
[ 14.298428] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 14.305912] usb usb2: Product: xHCI Host Controller
[ 14.310989] usb usb2: Manufacturer: Linux 5.10.168-g2c23e6c538 xhci-hcd
[ 14.317740] usb usb2: SerialNumber: xhci-hcd.0.auto
[ 14.323938] hub 2-0:1.0: USB hub found
[ 14.328891] hub 2-0:1.0: config failed, hub doesn't have any ports! (err -19)
[ 14.339539] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 14.346228] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
[ 14.354762] xhci-hcd xhci-hcd.1.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000000000010010
[ 14.364966] xhci-hcd xhci-hcd.1.auto: irq 493, io mem 0x31100000
[ 14.371736] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 14.377848] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
[ 14.386160] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 14.393537] usb usb3: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 14.402068] usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 14.409881] usb usb3: Product: xHCI Host Controller
[ 14.414974] usb usb3: Manufacturer: Linux 5.10.168-g2c23e6c538 xhci-hcd
[ 14.421738] usb usb3: SerialNumber: xhci-hcd.1.auto
[ 14.428021] hub 3-0:1.0: USB hub found
[ 14.432981] hub 3-0:1.0: 1 port detected
[ 14.440301] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
[ 14.449055] usb usb4: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10
[ 14.457632] usb usb4: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[* ] A start job is running for udev Wai鈥i[ 14.465763] usb usb4: Product: xHCI Host Controller
ce Initialization (8s / 3min 1s)
[ 14.475995] usb usb4: Manufacturer: Linux 5.10.168-g2c23e6c538 xhci-hcd
[ 14.485780] usb usb4: SerialNumber: xhci-hcd.1.auto
[ 14.492095] hub 4-0:1.0: USB hub found
[ 14.497094] hub 4-0:1.0: config failed, hub doesn't have any ports! (err -19)
[ 14.544489] usb 1-1: new low-speed USB device number 2 using xhci-hcd
[ 14.696386] usb 3-1: new high-speed USB device number 2 using xhci-hcd
[ 14.706488] usb 1-1: New USB device found, idVendor=046d, idProduct=c077, bcdDevice=72.00
[ 14.714686] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 14.722297] usb 1-1: Product: USB Optical Mouse
[ 14.726997] usb 1-1: Manufacturer: Logitech
[ 14.810031] input: Logitech USB Optical Mouse as /devices/platform/bus@f0000/f900000.dwc3-usb/31000000.usb/xhci-hcd.0.auto/usb1/1-1/1-1:1.0/0003:046D:C077.0001/input/input0
[ 14.825883] hid-generic 0003:046D:C077.0001: input: USB HID v1.11 Mouse [Logitech USB Optical Mouse] on usb-xhci-hcd.0.auto-1/input0
[ 14.842926] usbcore: registered new interface driver usbhid
[ 14.848615] usbhid: USB HID core driver
[ 14.856810] usb 3-1: New USB device found, idVendor=1a40, idProduct=0101, bcdDevice= 1.11
[ 14.872629] usb 3-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0
[ 14.886354] usb 3-1: Product: USB 2.0 Hub
[ 14.937846] hub 3-1:1.0: USB hub found
[ ***] A start job is running for udev Wai鈥ce Initialization (25s / 3min 1s)
[ 31.844381] vdd_mmc1: disabling
[FAILED] Failed to start udev Wait 鈥mplete Device Initialization.
See 'systemctl status systemd-udev-settle.service' for details.
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily rotation of log files.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API.
[ OK ] Listening on dropbear.socket.
Starting Reboot and dump vmcore via kexec...
[ OK ] Listening on Docker Socket for the API.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ OK ] Started autorun.
[ OK ] Started autorun2.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting rc.pvr.service...
Starting startwlansta...
Starting Login Service...
[ OK ] Started TEE Supplicant.
[ OK ] Started Reboot and dump vmcore via kexec.
[ OK ] Started startwlansta.
[ 129.015036] FAT-fs (mmcblk1p1): utf8 is not a recommended IO charset for FAT filesystems, filesystem will be case sensitive!
[ OK ] Started IPv6 Packet Filtering Framework.
[ OK ] Started IPv4 Packet Filtering Framework.
[ OK ] Reached target Network (Pre).
Starting Network Service...
[ 129.198691] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ OK ] Listening on Load/Save RF 鈥tch Status /dev/rfkill Watch.
[ 129.676833] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 129.781775] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ OK ] Started Network Service.
Starting Wait for Network to be Configured...
Starting Network Name Resolution...
[ 130.100800] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:01] driver [Generic PHY] (irq=POLL)
[ 130.208200] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rmii link mode
[ 130.368961] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:02] driver [Generic PHY] (irq=POLL)
[ 130.453039] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rmii link mode
[ OK ] Started Login Service.
[ 131.144666] startwlansta.sh[605]: Wi-Fi user configuration file missing, exit
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
Starting Avahi mDNS/DNS-SD Stack...
Starting Enable and configure wl18xx bluetooth stack...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Simple Network Ma鈥nt Protocol (SNMP) Daemon....
Starting Permit User Sessions...
[ OK ] Started Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
[ OK ] Started Enable and configure wl18xx bluetooth stack.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ 132.324816] am65-cpsw-nuss 8000000.ethernet eth1: Link is Up - 100Mbps/Full - flow control off
[ 132.333508] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
[ 132.580853] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 132.589782] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ OK ] Started Synchronize System and HW clocks.
[ OK ] Started Simple Network Man鈥ment Protocol (SNMP) Daemon..
[ OK ] Started rc.pvr.service.
Starting weston.service...
[ OK ] Started weston.service.
Starting telnetd.service...
[ OK ] Started telnetd.service.
Starting hmi_demo.service...
Starting LSB: Expand Rootfs of boot device...
[ OK ] Started LSB: Expand Rootfs of boot device.
[ 134.416729] PVR_K: 728: RGX Firmware image 'rgx.fw.33.15.11.3' loaded
[ 134.509008] PVR_K: 728: Shader binary image 'rgx.sh.33.15.11.3' loaded
[ OK ] Started hmi_demo.service.
Stopping hmi_demo.service...
[ OK ] Stopped hmi_demo.service.
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gstreamer1.0-libav
gzip
hidapi
less
libasm1
libbfd
libdw1
libelf1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp10
libidn2-0
libmpc3
libmpfr6
libreadline-dev
libreadline8
libunistring2
m4-dev
m4
make
nettle
parted
tar
which
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project am62xx-evm ttyS2
Arago 2021.09 am62xx-evm ttyS2
am62xx-evm login: [ 148.848899] Initializing XFRM netlink socket
[ 152.639860] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 152.685885] Bridge firewalling registered
[ 155.706652] process 'docker/tmp/qemu-check626469655/check' started with executable stack
am62xx-evm login:
请问使用的是哪个版本SDK? 是否有参考下面的migrating文档。
https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/09_00_00_03/exports/docs/linux/Foundational_Components_Migration_Guide.html
你好,我使用的版本是sdkti-processor-sdk-linux-am62xx-evm-08.06.00.42,我已参考文档进行修改,系统是可以引导启动的,但是在内核启动过程中会出现 A start job is running for udev wait for Complete Device Initialization (.. s / 3min),等待一段时间后Failed to start udev Wait for Complete Device Initialization.然后继续启动系统完成,我试着屏蔽其他设备去编译验证,还是会出现这个问题
6254换到6251就改了uboot和内核设备树的cpu数量,其他都没有改动,原本以为是设备初始化的问题,然后一个个屏蔽设备验证,还是有这个问题
#include "k3-am62.dtsi"
/ {
cpus {
#address-cells = <1>;
#size-cells = <0>;
cpu-map {
cluster0: cluster0 {
core0 {
cpu = <&cpu0>;
};
/*core1 {
cpu = <&cpu1>;
};
core2 {
cpu = <&cpu2>;
};
core3 {
cpu = <&cpu3>;
};*/
};
};
cpu0: cpu@0 {
compatible = "arm,cortex-a53";
reg = <0x000>;
device_type = "cpu";
enable-method = "psci";
i-cache-size = <0x8000>;
i-cache-line-size = <64>;
i-cache-sets = <256>;
d-cache-size = <0x8000>;
d-cache-line-size = <64>;
d-cache-sets = <128>;
next-level-cache = <&L2_0>;
operating-points-v2 = <&a53_opp_table>;
clocks = <&k3_clks 135 0>;
};
/*cpu1: cpu@1 {
compatible = "arm,cortex-a53";
reg = <0x001>;
device_type = "cpu";
enable-method = "psci";
i-cache-size = <0x8000>;
i-cache-line-size = <64>;
i-cache-sets = <256>;
d-cache-size = <0x8000>;
d-cache-line-size = <64>;
d-cache-sets = <128>;
next-level-cache = <&L2_0>;
operating-points-v2 = <&a53_opp_table>;
clocks = <&k3_clks 136 0>;
};
cpu2: cpu@2 {
compatible = "arm,cortex-a53";
reg = <0x002>;
device_type = "cpu";
enable-method = "psci";
i-cache-size = <0x8000>;
i-cache-line-size = <64>;
i-cache-sets = <256>;
d-cache-size = <0x8000>;
d-cache-line-size = <64>;
d-cache-sets = <128>;
next-level-cache = <&L2_0>;
operating-points-v2 = <&a53_opp_table>;
clocks = <&k3_clks 137 0>;
};
cpu3: cpu@3 {
compatible = "arm,cortex-a53";
reg = <0x003>;
device_type = "cpu";
enable-method = "psci";
i-cache-size = <0x8000>;
i-cache-line-size = <64>;
i-cache-sets = <256>;
d-cache-size = <0x8000>;
d-cache-line-size = <64>;
d-cache-sets = <128>;
next-level-cache = <&L2_0>;
operating-points-v2 = <&a53_opp_table>;
clocks = <&k3_clks 138 0>;
};*/
};
a53_opp_table: opp-table {
compatible = "operating-points-v2-ti-cpu";
opp-shared;
syscon = <&wkup_conf>;
opp-200000000 {
opp-hz = /bits/ 64 <200000000>;
opp-supported-hw = <0x01 0x0007>;
clock-latency-ns = <6000000>;
opp-suspend;
};
opp-400000000 {
opp-hz = /bits/ 64 <400000000>;
opp-supported-hw = <0x01 0x0007>;
clock-latency-ns = <6000000>;
};
opp-600000000 {
opp-hz = /bits/ 64 <600000000>;
opp-supported-hw = <0x01 0x0007>;
clock-latency-ns = <6000000>;
};
opp-800000000 {
opp-hz = /bits/ 64 <800000000>;
opp-supported-hw = <0x01 0x0007>;
clock-latency-ns = <6000000>;
};
opp-1000000000 {
opp-hz = /bits/ 64 <1000000000>;
opp-supported-hw = <0x01 0x0006>;
clock-latency-ns = <6000000>;
};
opp-1250000000 {
opp-hz = /bits/ 64 <1250000000>;
opp-supported-hw = <0x01 0x0004>;
clock-latency-ns = <6000000>;
};
};
L2_0: l2-cache0 {
compatible = "cache";
cache-level = <2>;
cache-size = <0x40000>;
cache-line-size = <64>;
cache-sets = <512>;
};
};
对于从6254到6251的迁移,只是核心数量不同一般不需要修改设备树,直接就可以运行,驱动会根据检测到的soc id来判定是几个核,也就是说直接使用 k3-am625.dtsi 这个dtsi就可以了,你是已经试过不行吗?
请看下面e2e工程师的回复。
Will you have a look at the FAQ, especially on RTI_WDT error.
e2e.ti.com/.../faq-am62ax-am62x-am64x-rti_wdt_probe-error-on-linux-boot