This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2SX: MMCAS-RF-EVM,MMCAS-DSP-EVM 下载FPGA固件出现问题

Part Number: TDA2SX


我使用HW-USBN-2B下载器,在diamond programmer软件进行下载。出现问题如下:

1、使用SSPI SRAM下载可以正常下载,如下图:

2、使用SPI FLASH下载出现报错,如下图:

疑问1:第一种方法能下载,说明不是下载器和接线的问题,我使用下面这个配置进行下载就会出现报错,可能的问题是什么?

疑问2:我下载FPGA固件的原因是想验证一下这个固件,我们团队基于MMCAS-DSP-EVM的设计文件做了一块板,所以需要验证固件是否可以用,TI的FPGA固件否是通过上面的问题2中的下载方式下载到挂在FPGA芯片上面的nor flash上,这样子就可以做到一次性下载?