This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

vpif



你好,目前我使用DM6467T和FPGA通信,采用VPIF接口,BT1120,采用隔场扫描方式,YC分离模式,L1=1,L3=45,L5=813,L7=818,L9=862,L11=1246

但是dm6467只能收到CH0和CH1的TOP FIELD的数据,bottom field 数据收不到,还有就是在中断函数中,添加打印CH0寄存器的第5位,也就是判断顶场和底场的

的,显示一直为1,也就是一直识别的是底场,重来没有置0,CH0和CH1寄存器的第6位和第7位,无论改成任何模式,现象都是和我上面的描述一样