This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have recently started working with TMS320C6748, and I am troubled by this statement in the routine about SPI. I cannot understand the role of HWREG and what the overall meaning of this function is. I hope you can answer for me.
The code you've provided is written in C and appears to be a function named SPIReset, which takes an unsigned integer baseAdd as a parameter. This function seems to reset the SPI module by writing a value to the SPIGCR0 register.
The HWREG macro is often used in embedded systems programming to access and manipulate hardware registers. It is typically defined as a macro that allows direct access to memory-mapped hardware registers. In this context, HWREG is being used to access the memory address corresponding to the baseAdd offset by SPI_SPIGCR0, and then a value is written to that memory address.
The expression HWREG(baseAdd + SPI_SPIGCR0) is accessing the memory-mapped register at the address baseAdd + SPI_SPIGCR0, and then the value ~(SPI_SPIGCR0_RESET) is being assigned to that register.
The ~(SPI_SPIGCR0_RESET) seems to be a bitwise negation of the value SPI_SPIGCR0_RESET. The purpose of this code is likely to reset specific bits or flags within the SPIGCR0 register.
Yes, that is correct. After executing the "SPIReset" function, the register at the address (baseAdd + SPI_SPIGCR0) will be assigned the value of ~(SPI_SPIGCR0_RESET). The tilde (~) operator performs a bitwise negation, so it will invert the bits of the value SPI_SPIGCR0_RESET and then assign the result to the specified register. This operation is likely intended to reset or initialize the SPI control register to a specific value.
You are welcome, this is what I should do, I will close this post, if you have any questions, please post again, thank you
Hello, this post has been closed, please post again to exchange, thank you for understanding, thank you