This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 LCDK NANDWrite

Other Parts Discussed in Thread: OMAP-L138

现在想把DSP程序固化到NAND FLASH里,有没有对应的NANDWriter工程或可执行文件?

  • 看一下这里面的路径中:

    mcsdk_1_01_00_02/host-tools/OMAP-L138_FlashAndBootUtils_2.40/OMAP-L138/CCS/NANDWriter/src/nandwriter.c

  • 你好

    1.我在wiki上看到关于138 MCSDK里写到

    For a Windows host, run the mcsdk_<build-id>_windows_setup.exe executable.

    但是实际文件夹中只有C:\ti\mcsdk_1_01_00_02\setup.sh

    请问我该怎么处理?

    2.我安装的MCSDK 是不是对的?mcsdk_1_01_00_02

    3.安装的一些文件夹主要有什么用?

    pdk_OMAPL138_1_01_00_02

    syslink_2_21_01_05

    dsplib_c674x_3_1_1_1

    又没有这方面比较好的教程?

    4.MCSDK和starterware之间有什么区别?

    5.手头上有一个L138的LCDK 到底该如何入手!!!!!!

    非常感谢!