This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于am335x sdk7.0烧写emmc的问题

各位大牛,急需帮忙:

        就是我sdk6.0已经可以烧写了,按照那个方法烧写sdk7.0也能烧写好,可是让板子自己启动的时候u-boot阶段出现了问题。log如下:

reading uEnv.txt                                                                
** Unable to read file uEnv.txt **                                              
reading uImage                                                                  
4117904 bytes read in 406 ms (9.7 MiB/s)                                        
Booting from mmc ...                                                            
## Booting kernel from Legacy Image at 80007fc0 ...                             
   Image Name:   Linux-3.12.10-ti2013.12.01                                     
   Image Type:   ARM Linux Kernel Image (uncompressed)                          
   Data Size:    4117840 Bytes = 3.9 MiB                                        
   Load Address: 80008000                                                       
   Entry Point:  80008000                                                       
   Verifying Checksum ... OK                                                    
   XIP Kernel Image ... OK                                                      
OK                                                                              
                                                                                
Starting kernel ...  

请问这个uEnv.txt 如何生成呢?