This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678芯片内阻

TI的工程师,您好,

       我现在在调试TI C6678,自己做的板子,买了一个芯片版本1.0,对比版本2.0,测了一下内阻,发现了一个问题,测得CVDD与VSS之间内阻为2.5欧姆,而2.0版本的那个芯片CVDD与VSS之间电阻测的是24.5,其他的CVDD1分别为45.3欧姆和96.6欧姆,CVDD15分别为6.89K和7.72K,CVDD18分别为6.08K和6.94K。看起来只有CVDD和CVDD1的相差较大,尤其是CVDD,买的那个芯片基本上就是CVDD与VSS时间电阻值很小,请问这是正常的吗?会不会是DSP里面坏了所以才会出现这样的情况?6678的内阻范围在芯片资料中能够查到吗?

希望尽快回复,谢谢!