GS2971和GV7601是同类芯片,如果您用的是GV7601,也请帮我一下。
应用程序:DVRDK的demos里面的link_api_demos。
30HZ:GS2971采用的是10bit模式连接到DM8168,实际上用了其中的8bit。目前采集30帧没有问题,h264压缩码率在6M也没有出现问题。
60HZ:GS2971采用的是20bit模式连接到DM8168,实际上用了其中的16bit。没有任何图像显示。
我想问一下,GS2971在30HZ采集和60HZ采集两种模式,在寄存器设置方面有什么不同(我在datasheet里面没发现什么不同啊)?link_api_demos是不是也要有相关的修改呢?改哪里?