Part Number: AM5718
专家们好,
我这边CPU是am5718,用linux系统,产品以太网需要用自己的mac地址,我需要如何做才能将自己的mac地址用在板卡。用的是两个千兆以太网。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 打开终端,使用以下命令查看当前网络接口的MAC地址:
ifconfig
2. 确定您想要使用的MAC地址,并将其记录下来。
3. 编辑网络接口的配置文件,将您想要使用的MAC地址添加到配置文件中。例如,如果您使用的是eth0接口,可以使用以下命令编辑配置文件:
sudo nano /etc/network/interfaces
在配置文件中找到对应的网络接口配置,然后添加以下内容:
hwaddress ether 00:11:22:33:44:55
其中“00:11:22:33:44:55”是您想要使用的MAC地址。
4. 保存并退出配置文件,然后重新启动网络服务以使更改生效:
sudo systemctl restart networking
5. 使用以下命令验证MAC地址是否已更改:
ifconfig