This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 MAC地址发生改变



    TI的各位专家:

                              你们好!我们在使用8168的过程中发现了一个比较严重的问题,我们发现系统运行过程中,mac地址突然变掉,因为我们用交换机绑定了mac地址,有时候未做任何操作,但交换机检测到系统的mac地址发生了改变,导致网络出现异常。过一会可能就恢复了。下图为我们的实验数据,因为我们的产品涉及到网络安全,所以必须用交换机来绑定mac地址。该问题导致系统运行一段时间就异常。无法使用。所以麻烦各位专家帮忙诊断下。 另外我们使用的DVRRDK4.0的开发包,即使不跑我们自己的业务,我们发现也有该问题。期待您们的回复,谢谢!

             

设备名称

原始MAC地址

连接的交换机端口

1MAC变化

重新将端口启用后,2MAC变化

重新将端口启用后,3MAC变化

192.168.71.1-解码盒

9059-af6b-982a

GE1/0/13

36:37:38:39:30:31

BA:4C:12:00:00:00

 

192.168.71.2-解码盒

9059-af6b-7748

GE1/0/4

36:37:38:39:30:31

 

 

192.168.71.3-解码盒

1cba-8ccc-4a7a

GE1/0/2

36:37:38:39:30:31

0A:6A:0D:00:00:00

 

192.168.71.4-解码盒

1cba-8ccd-119a

GE1/0/16

36:37:38:39:30:31

36:37:38:39:30:31

6C:65:6E:3D:31:37

192.168.71.11-编码盒

1cba-8ccc-4a2c

GE1/0/7

36:37:38:39:30:31

36:37:38:39:30:31

48:EB:AC:17:CD:6D

192.168.71.12-编码盒

1cba-8ccc-72c6

GE1/0/8

BC:80:11:00:00:00

A6:AF:1B:00:00:00