This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 平台下openMP程序应该如何加载?



    大家好,我在C6678 EVM上运行ti提供的opemMP的例程,编译成功了。但是生成的out文件到底应该如何正确的加载呢?

    例程的user guide上只写了要connect core0,然后将out文件load到core0上,之后run,core0会自动的调度其他的core1~3(例程中用了4个core)运行各自的任务。但是我这样操作之后core0一直出去running状态,但是其他core没有反应。
    于是我又把所有的core0~3全connect上了,然后将out文件load到core0上,之后点击core0  并RUN,但是还是没有正确的运行。
请问opemmp程序,应该如何正确的连接,加载和运行?
谢谢大家!