This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6446 ARM端中断



您好,我在测试DM6446,ARM端的(引脚)外部中断(官网下载的例子程序,路径:davincievm\csl\arm\example\intc)时不能进入中断。所以函数都能正确执行,但是就是无法进入中断,我也尝试过其他的例子程序,都不能进入中断,这是怎么回事,请指点一二,万分感激!!!

SWI_sysMode();

/* Initialize INTC */
CSL_intcInit();

/* Initialize INTC Dispatcher */
CSL_intcDispatcherInit();

/* Enable all interrupts */
CSL_intcGlobalEnable(&eventStat);

/* Open INTC */
gpioIntcHwSetup.priority = CSL_INTC_PRIORITY_2;
gpioIntcHandle = CSL_intcOpen(&gpioIntcObj, CSL_INTC_EVENTID_GPIO0,
CSL_INTC_VECTID_DEFAULT, &gpioIntcHwSetup, &status);

/* HwSetup INTC */
CSL_intcHwSetup(gpioIntcHandle, &gpioIntcHwSetup);

/* Bind ISR HandleGPIO_INT to Interrupt Controller */
isr_gpio.handler = HandleGPIO_INT;
isr_gpio.arg = NULL;
CSL_intcPlugEventHandler(gpioIntcHandle, &isr_gpio);

/* Event Enable */
CSL_intcEventEnable(CSL_INTC_EVENTID_GPIO0, &eventStat);

printf ("\nINTC: Interrupt Controller Setup... Passed.\n");
status = CSL_SOK;
/* Initialize the GPIO CSL module */
status = CSL_gpioInit(&pContext);
status = CSL_SOK;
if (status != CSL_SOK) {
printf ("GPIO: Initialization... Failed.\n");
return;
}
else {
printf ("GPIO: Module Initialization... Passed.\n");
}

/* Open the CSL module */
hGpio = CSL_gpioOpen(&gpioObj, CSL_GPIO, NULL, &status);
if ((hGpio == NULL) || (status != CSL_SOK)) {
printf ("GPIO: Module Open... Failed.\n");
return;
}
else {
hGpio->numBanks = CSL_GPIO_NUM_BANKS;
hGpio->numPins = CSL_GPIO_NUM_PINS;
printf ("GPIO: Module open... Passed.\n");
}

/* Setup hardware parameters */
hwSetup.extendSetup = NULL;

/* Setup the General Purpose IO */
status = CSL_gpioHwSetup(hGpio, &hwSetup);

printf ("GPIO: Module Setup... Passed.\n");

/* Interrupt Generation indicator flag is reset */
IntGenFlag = 0;

/* Configure pins 0 & 8 to generate an interrupt on Rising Edge, and
* configure it as an output, then set the data High (Low->High).
* Set Trigger
*/
// status = CSL_gpioHwControl(hGpio, CSL_GPIO_CMD_BANK_INT_ENABLE, &banknumber);
hGpio->regs->BINTEN = 1;
config.pinNum = CSL_GPIO_PIN0;
config.trigger = CSL_GPIO_TRIG_RISING_EDGE;
config.direction = CSL_GPIO_DIR_OUTPUT;

status = CSL_gpioHwControl(hGpio, CSL_GPIO_CMD_CONFIG_BIT, &config);
if (status != CSL_SOK) {
printf ("GPIO: Command to GPIO configuration... Failed.\n");
errorExit();
}

config.pinNum = CSL_GPIO_PIN8;
config.trigger = CSL_GPIO_TRIG_RISING_EDGE;
config.direction = CSL_GPIO_DIR_OUTPUT;
status = CSL_gpioHwControl(hGpio, CSL_GPIO_CMD_CONFIG_BIT, &config);
if (status != CSL_SOK) {
printf ("GPIO: Command to GPIO configuration... Failed.\n");
errorExit();
}

/* Set Data High: */
pinNum = CSL_GPIO_PIN0;
status = CSL_gpioHwControl(hGpio, CSL_GPIO_CMD_CLEAR_BIT, &pinNum);
if (status != CSL_SOK) {
printf ("GPIO: Command to set bit... Failed.\n");
errorExit();
}
/*
pinNum = CSL_GPIO_PIN0;
status = CSL_gpioHwControl(hGpio, CSL_GPIO_CMD_SET_BIT, &pinNum);
if (status != CSL_SOK) {
printf ("GPIO: Command to set bit... Failed.\n");
errorExit();
}
*/
pinNum = CSL_GPIO_PIN8;
status = CSL_gpioHwControl(hGpio, CSL_GPIO_CMD_CLEAR_BIT, &pinNum);
if (status != CSL_SOK) {
printf ("GPIO: Command to set bit... Failed.\n");
errorExit();
}

printf ("GPIO: Condition for interrupt generation... Done.\n");

/* Wait for interrupt to be generated.
* On receiving the interrupt, the CPU control goes to the ISR
* In the ISR, the variable IntGenFlag becomes 1
*/
pinNum = CSL_GPIO_PIN0;
while (IntGenFlag == 0)
{
DAVINCIEVM_wait(10000);
status = CSL_gpioHwControl(hGpio, CSL_GPIO_CMD_SET_BIT, &pinNum);
DAVINCIEVM_wait(10000);
status = CSL_gpioHwControl(hGpio, CSL_GPIO_CMD_CLEAR_BIT, &pinNum);
}

printf ("\nGPIO: Interrupt Occurred.\n");

/* Check Interrupt Status: */
bankData.data = 0;
bankData.index = 0;
status = CSL_gpioHwControl(hGpio, CSL_GPIO_CMD_GET_INTSTATUS, &bankData);
if (status != CSL_SOK) {
printf ("GPIO: Command to GPIO configuration... Failed.\n");
errorExit();
}

if (bankData.data != 0x00000101){
printf ("\nError in Interrupt Loopback Path\n");
}

/* Close the opened instances of GPIO and INTC */
CSL_gpioClose (hGpio);
CSL_intcClose (gpioIntcHandle);