This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

vpfe-capture vpfe-capture: stream off failed in subdev

Other Parts Discussed in Thread: TVP7002

我在dm368上移植dvsdk4.02后,测试demo,运行信息如下:

./encode -v test.264 -y 5 -I 3

Encode demo started......
davinci_resizer davinci_resizer.2: RSZ_G_CONFIG:0:1:124
davinci_previewer davinci_previewer.2: ipipe_set_preview_config
vpfe-capture vpfe-capture: IPIPE Chained
vpfe-capture vpfe-capture: Resizer present
EVM: switch to tvp7002 HD video input
vpfe-capture vpfe-capture: width = 1920, height = 1080, bpp = 1
vpfe-capture vpfe-capture: adjusted width = 1920, height = 1080, bpp = 1, bytesp
erline = 1920, sizeimage = 3110400
vpfe-capture vpfe-capture: width = 1920, height = 1080, bpp = 1
vpfe-capture vpfe-capture: adjusted width = 1920, height = 1080, bpp = 1, bytesp
erline = 1920, sizeimage = 3110400
davinci_v4l2 davinci_v4l2.1: Before finishing with S_FMT:
layer.pix_fmt.bytesperline = 1920,
 layer.pix_fmt.width = 1920,
 layer.pix_fmt.height = 1080,
 layer.pix_fmt.sizeimage =3110400
davinci_v4l2 davinci_v4l2.1: pixfmt->width = 1920,
 layer->layer_info.config.line_length= 1920
ARM Load: 10% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 0 kbps Tim
e: 00:00:01 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolution: 1
920x1080 Sound Codec: N/A Sampling Freq: N/A


ARM Load: 0% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 0 kbps Time
: 00:00:06 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolution: 19
20x1080 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 0% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 0 kbps Time
: 00:00:07 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolution: 19
20x1080 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 0% Video fps: 0 fps Video bit rate: 0 kbps Sound bit rate: 0 kbps Time
: 00:00:08 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolution: 19
20x1080 Sound Codec: N/A Sampling Freq: N/A

我用Crtl + c 键终止运行后弹出如下信息:

tvp7002 1-005d: Write: retry ... 1
tvp7002 1-005d: Write: retry ... 2
tvp7002 1-005d: Write: retry ... 3
tvp7002 1-005d: Unable to turn off decoder
vpfe-capture vpfe-capture: stream off failed in subdev

请问为什么编码一直是0% 呢,运行有什么不对的地方么? 请给予指点,十分感谢