This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM8168 EZSDK5.03.01.15 SYSLINK SAMPLES



大家好!

 请问用使用EZSDK evm_5_03_01_15开发包时候是否遇到 syslink samples例程不能运行,现在我使用evm_5_03_01_15包中的u-boot uImage 以及它的文件系统制作SD卡启动盘,启动之后运行syslink samples 例程的时候报了一堆内存的错误。 在网上也没有找到解决方法,请问是需要修改什么配置吗?运行syslink samples 例程的步骤也是按照手册上来做的。

  • Xshell for Xmanager Enterprise 3.0 (Build 0249)

    Copyright (c) 2002-2009 NetSarang Computer, Inc. All rights reserved.

    Type `help' to learn how to use Xshell prompt.

    Xshell:\>

    Connecting to COM3...

    Connected.

                                                                                       0

    raise: Signal # 8 caught

    reading boot.scr

    301 bytes read

    Running bootscript from MMC/SD to set the ENV...

    ## Executing script at 80900000

    reading uImage

    2428376 bytes read

    ## Booting kernel from Legacy Image at 80009000 ...

      Image Name:   Arago/2.6.37-psp04.00.01.13/dm81

      Image Type:   ARM Linux Kernel Image (uncompressed)

      Data Size:    2428312 Bytes = 2.3 MiB

      Load Address: 80008000

      Entry Point:  80008000

      Verifying Checksum ... OK

      Loading Kernel Image ... OK

    OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.

    Linux version 2.6.37 (x0029463@swubn01) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 Fri Dec 9 11:59:08 IST 2011

    CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f

    CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

    Machine: ti8168evm

    bootconsole [earlycon0] enabled

    vram size = 52428800 at 0x0

    reserved size = 52428800 at 0x0

    FB: Reserving 52428800 bytes SDRAM for VRAM

    Memory policy: ECC disabled, Data cache writeback

    OMAP chip is TI8168 1.1

    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 52224

    Kernel command line: console=ttyO2,115200n8 rootwait root=/dev/mmcblk0p2 rw mem=256M earlyprintk notifyk.vpssm3_sva=0xBF900000 vram=50M ti816xfb.vram=0:16M,1:16M,2:6M ip=off noinitrd

    PID hash table entries: 1024 (order: 0, 4096 bytes)

    Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)

    Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)

    Memory: 206MB = 206MB total

    Memory: 203420k/203420k available, 58724k reserved, 0K highmem

    Virtual kernel memory layout:

       vector  : 0xffff0000 - 0xffff1000   (   4 kB)

       fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

       DMA     : 0xffc00000 - 0xffe00000   (   2 MB)

       vmalloc : 0xd0800000 - 0xf8000000   ( 632 MB)

       lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)

       pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

       modules : 0xbf000000 - 0xbfe00000   (  14 MB)

         .init : 0xc0008000 - 0xc003a000   ( 200 kB)

         .text : 0xc003a000 - 0xc049c000   (4488 kB)

         .data : 0xc049c000 - 0xc04e36c0   ( 286 kB)

    SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

    NR_IRQS:407

    IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts

    Total of 128 interrupts on 1 active controller

    GPMC revision 6.0

    Trying to install interrupt handler for IRQ400

    Trying to install interrupt handler for IRQ401

    Trying to install interrupt handler for IRQ402

    Trying to install interrupt handler for IRQ403

    Trying to install interrupt handler for IRQ404

    Trying to install interrupt handler for IRQ405

    Trying to install interrupt handler for IRQ406

    Trying to install type control for IRQ407

    Trying to set irq flags for IRQ407

    OMAP clockevent source: GPTIMER1 at 27000000 Hz

    Console: colour dummy device 80x30

    Calibrating delay loop... 986.31 BogoMIPS (lpj=4931584)

    pid_max: default: 32768 minimum: 301

    Security Framework initialized

    Mount-cache hash table entries: 512

    CPU: Testing write buffer coherency: ok

    devtmpfs: initialized

    omap_voltage_early_init: voltage driver support not added

    regulator: core version 0.5

    regulator: dummy:

    NET: Registered protocol family 16

    OMAP GPIO hardware version 0.1

    OMAP GPIO hardware version 0.1

    omap_mux_init: Add partition: #1: core, flags: 0

    _omap_mux_get_by_name: Could not find signal i2c2_scl.i2c2_scl

    _omap_mux_get_by_name: Could not find signal i2c2_sda.i2c2_sda

    NOR: Can't request GPMC CS

    registered ti816x_vpss device

    registered ti816x_gpio_vr device

    registered TI816x on-chip HDMI device

    registered ti816x_sr device

    registered ti81xx_vidout device

    pm_dbg_init: only OMAP3 supported

    ti81xx_pcie: Invoking PCI BIOS...

    ti81xx_pcie: Setting up Host Controller...

    ti81xx_pcie: Register base mapped @0xd0820000

    ti81xx_pcie: Starting PCI scan...

    PCI: bus0: Fast back to back transfers enabled

    bio: create slab <bio-0> at 0

    regulator: VFB: 800 <--> 1025 mV at 1010 mV

    vgaarb: loaded

    SCSI subsystem initialized

    usbcore: registered new interface driver usbfs

    usbcore: registered new interface driver hub

    usbcore: registered new device driver usb

    registerd cppi-dma Intr @ IRQ 17

    Cppi41 Init Done

    omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz

    omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz

    Advanced Linux Sound Architecture Driver Version 1.0.23.

    Switching to clocksource gp timer

    musb-hdrc: version 6.0, host, debug=0

    musb-hdrc musb-hdrc.0: dma type: dma-cppi41

    musb-hdrc: kernel must blacklist external hubs

    musb-hdrc musb-hdrc.0: MUSB HDRC host driver

    musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1

    usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

    usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

    usb usb1: Product: MUSB HDRC host driver

    usb usb1: Manufacturer: Linux 2.6.37 musb-hcd

    usb usb1: SerialNumber: musb-hdrc.0

    hub 1-0:1.0: USB hub found

    hub 1-0:1.0: 1 port detected

    musb-hdrc musb-hdrc.0: USB Host mode controller at d081e000 using DMA, IRQ 18

    musb-hdrc musb-hdrc.1: dma type: dma-cppi41

    musb-hdrc: kernel must blacklist external hubs

    musb-hdrc musb-hdrc.1: MUSB HDRC host driver

    musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2

    usb usb2: New USB device found, idVendor=1d6b, idProduct=0002

    usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1

    usb usb2: Product: MUSB HDRC host driver

    usb usb2: Manufacturer: Linux 2.6.37 musb-hcd

    usb usb2: SerialNumber: musb-hdrc.1

    hub 2-0:1.0: USB hub found

    hub 2-0:1.0: 1 port detected

    musb-hdrc musb-hdrc.1: USB Host mode controller at d0826800 using DMA, IRQ 19

    NET: Registered protocol family 2

    IP route cache hash table entries: 2048 (order: 1, 8192 bytes)

    TCP established hash table entries: 8192 (order: 4, 65536 bytes)

    TCP bind hash table entries: 8192 (order: 3, 32768 bytes)

    TCP: Hash tables configured (established 8192 bind 8192)

    TCP reno registered

    UDP hash table entries: 256 (order: 0, 4096 bytes)

    UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

    NET: Registered protocol family 1

    RPC: Registered udp transport module.

    RPC: Registered tcp transport module.

    RPC: Registered tcp NFSv4.1 backchannel transport module.

    NetWinder Floating Point Emulator V0.97 (double precision)

    PMU: registered new PMU device of type 0

    omap-iommu omap-iommu.0: ducati registered

    omap-iommu omap-iommu.1: sys registered

    JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.

    msgmni has been set to 397

    io scheduler noop registered

    io scheduler deadline registered

    io scheduler cfq registered (default)

    Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

    omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0

    omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1

    omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2

    console [ttyO2] enabled, bootconsole disabled

    console [ttyO2] enabled, bootconsole disabled

    brd: module loaded

    loop: module loaded

    ahci ahci.0: forcing PORTS_IMPL to 0x3

    ahci ahci.0: AHCI 0001.0100 32 slots 2 ports 3 Gbps 0x3 impl platform mode

    ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc

    scsi0 : ahci_platform

    scsi1 : ahci_platform

    ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16

    ata2: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x180 irq 16

    m25p80 spi1.0: found m25p05-nonjedec, expected w25x32

    m25p80 spi1.0: m25p05-nonjedec (64 Kbytes)

    Creating 4 MTD partitions on "spi_flash":

    0x000000000000-0x000000040000 : "U-Boot"

    mtd: partition "U-Boot" extends beyond the end of device "spi_flash" -- size truncated to 0x10000

    0x000000010000-0x000000012000 : "U-Boot Env"

    mtd: partition "U-Boot Env" is out of reach -- disabled

    0x000000000000-0x000000280000 : "Kernel"

    mtd: partition "Kernel" extends beyond the end of device "spi_flash" -- size truncated to 0x10000

    0x000000010000-0x000000010000 : "File System"

    mtd: partition "File System" is out of reach -- disabled

    omap2-nand driver initializing

    NAND device: Manufacturer ID: 0x6c, Chip ID: 0x53 (Unknown )

    Creating 5 MTD partitions on "omap2-nand.0":

    0x000000000000-0x000000260000 : "U-Boot"

    0x000000260000-0x000000280000 : "U-Boot Env"

    0x000000280000-0x0000006c0000 : "Kernel"

    0x0000006c0000-0x00000cee0000 : "File System"

    mtd: partition "File System" extends beyond the end of device "omap2-nand.0" -- size truncated to 0x940000

    0x000001000000-0x000001000000 : "Reserved"

    mtd: partition "Reserved" is out of reach -- disabled

    davinci_mdio davinci_mdio.0: davinci mdio revision 1.6

    davinci_mdio davinci_mdio.0: detected phy mask fffffff9

    davinci_mdio.0: probed

    davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown

    davinci_mdio davinci_mdio.0: phy[2]: device 0:02, driver unknown

    usbcore: registered new interface driver cdc_ether

    usbcore: registered new interface driver dm9601

    Initializing USB Mass Storage driver...

    usbcore: registered new interface driver usb-storage

    USB Mass Storage support registered.

    mice: PS/2 mouse device common for all mice

    omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0

    i2c /dev entries driver

    Linux video capture interface: v2.00

    usbcore: registered new interface driver uvcvideo

    USB Video Class driver (v1.0.0)

    OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec

    usbcore: registered new interface driver usbhid

    usbhid: USB HID core driver

    notify_init : notify drivercreated  for  remote proc id 2 at physical Address 0xbf900000

    usbcore: registered new interface driver snd-usb-audio

    asoc: tlv320aic3x-hifi <-> davinci-mcasp.2 mapping ok

    ALSA device list:

     #0: TI81XX EVM

    TCP cubic registered

    NET: Registered protocol family 17

    VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3

    omap_voltage_late_init: Voltage driver support not added

    Power Management for TI81XX.

    smartreflex smartreflex: Driver initialized

    omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)

    ata2: SATA link down (SStatus 0 SControl 300)

    ata1: SATA link down (SStatus 0 SControl 300)

    Waiting for root device /dev/mmcblk0p2...

    mmc0: new high speed SDHC card at address b368

    mmcblk0: mmc0:b368 SD4GB 3.74 GiB

    mmcblk0: p1 p2 p3

    EXT3-fs: barriers not enabled

    kjournald starting.  Commit interval 5 seconds

    EXT3-fs (mmcblk0p2): using internal journal

    EXT3-fs (mmcblk0p2): recovery complete

    EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode

    VFS: Mounted root (ext3 filesystem) on device 179:2.

    devtmpfs: mounted

    Freeing init memory: 200K

    INIT: version 2.86 booting

    Please wait: booting...

    Error opening /dev/fb0: No such file or directory

    Starting udev

    udevd (73): /proc/73/oom_adj is deprecated, please use /proc/73/oom_score_adj instead.

    EXT3-fs: barriers not enabled

    kjournald starting.  Commit interval 5 seconds

    EXT3-fs (mmcblk0p3): using internal journal

    EXT3-fs (mmcblk0p3): recovery complete

    EXT3-fs (mmcblk0p3): mounted filesystem with writeback data mode

    Remounting root file system...

    Caching udev devnodes

    NET: Registered protocol family 10

    ALSA: Restoring mixer settings...

    Configuring network interfaces... No state is present for card EVM

    Found hardware: "" "" "" "" ""

    Hardware is initialized using a generic method

    No state is present for card EVM

    davinci_mdio davinci_mdio.0: resetting idled controller

    net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f014)

    ADDRCONF(NETDEV_UP): eth0: link is not ready

    udhcpc (v1.13.2) started

    Sending discover...

    Sending discover...

    Sending discover...

    No lease, forking to background

    done.

    Setting up IP spoofing protection: rp_filter.

    Fri Dec  9 14:48:00 UTC 2011

    INIT: Entering runlevel: 5

    Loading HDVICP2 Firmware

    DM816X prcm_config_app version: 2.0.0.1

    Doing PRCM settings...

    PRCM for IVHD0 is in Progress, Please wait.....  

    BW Phy Addr : 0x48180600 Data : 0x00000002

    AW Phy Addr : 0x48180600 Data : 0x00000002

    Phy Addr : 0x48180c04 Data : 0x00000037

    BW Phy Addr : 0x48180620 Data : 0x00070000

    AW Phy Addr : 0x48180620 Data : 0x00070002

    BW Phy Addr : 0x48180624 Data : 0x00030000

    AW Phy Addr : 0x48180624 Data : 0x00010002

    Phy Addr : 0x48180600 Data : 0x00000102

    BW Phy Addr : 0x48180c10 Data : 0x00000007

    AW Phy Addr : 0x48180c10 Data : 0x00000003

    Phy Addr : 0x48180c14 Data : 0x00000004

    BW Phy Addr : 0x58088000 Data : 0x322bed97

    AW Phy Addr : 0x58088000 Data : 0xeafffffe

    BW Phy Addr : 0x58098000 Data : 0x913084a2

    AW Phy Addr : 0x58098000 Data : 0xeafffffe

    BW Phy Addr : 0x48180c10 Data : 0x00000003

    AW Phy Addr : 0x48180c10 Data : 0x00000000

    Phy Addr : 0x48180c14 Data : 0x00000007

    PRCM for IVHD0 is Done Successfully  

    PRCM for IVHD1 is in Progress, Please wait.....  

    BW Phy Addr : 0x48180700 Data : 0x00000002

    AW Phy Addr : 0x48180700 Data : 0x00000002

    Phy Addr : 0x48180d04 Data : 0x00000037

    BW Phy Addr : 0x48180720 Data : 0x00070000

    AW Phy Addr : 0x48180720 Data : 0x00050002

    BW Phy Addr : 0x48180724 Data : 0x00030000

    AW Phy Addr : 0x48180724 Data : 0x00010002

    Phy Addr : 0x48180700 Data : 0x00000102

    BW Phy Addr : 0x48180d10 Data : 0x00000007

    AW Phy Addr : 0x48180d10 Data : 0x00000003

    Phy Addr : 0x48180d14 Data : 0x00000004

    BW Phy Addr : 0x5a088000 Data : 0xeccb897c

    AW Phy Addr : 0x5a088000 Data : 0xeafffffe

    BW Phy Addr : 0x5a098000 Data : 0x38e389e2

    AW Phy Addr : 0x5a098000 Data : 0xeafffffe

    BW Phy Addr : 0x48180d10 Data : 0x00000003

    AW Phy Addr : 0x48180d10 Data : 0x00000000

    Phy Addr : 0x48180d14 Data : 0x00000007

    PRCM for IVHD1 is Done Successfully  

    PRCM for IVHD2 is in Progress, Please wait.....  

    BW Phy Addr : 0x48180800 Data : 0x00000002

    AW Phy Addr : 0x48180800 Data : 0x00000002

    Phy Addr : 0x48180e04 Data : 0x00000037

    BW Phy Addr : 0x48180820 Data : 0x00070000

    AW Phy Addr : 0x48180820 Data : 0x00050002

    BW Phy Addr : 0x48180824 Data : 0x00030000

    AW Phy Addr : 0x48180824 Data : 0x00010002

    Phy Addr : 0x48180800 Data : 0x00000102

    BW Phy Addr : 0x48180e10 Data : 0x00000007

    AW Phy Addr : 0x48180e10 Data : 0x00000003

    Phy Addr : 0x48180e14 Data : 0x00000004

    BW Phy Addr : 0x53088000 Data : 0xebaa6e81

    AW Phy Addr : 0x53088000 Data : 0xeafffffe

    BW Phy Addr : 0x53098000 Data : 0x96097bc9

    AW Phy Addr : 0x53098000 Data : 0xeafffffe

    BW Phy Addr : 0x48180e10 Data : 0x00000003

    AW Phy Addr : 0x48180e10 Data : 0x00000000

    Phy Addr : 0x48180e14 Data : 0x00000007

    PRCM for IVHD2 is Done Successfully  

    PRCM Initialization completed

    SysLink version : 2.00.05.85

    SysLink module created on Date:Dec  9 2011 Time:12:47:37

    FIRMWARE: Memory map bin file not passed

    Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]

    FIRMWARE: Default memory configuration is used

    MemCfg: DCMM (Dynamically Configurable Memory Map) Version :  2.1.1.1

    FIRMWARE: Memory Configuration status : In Progress

    FIRMWARE: 1 start Successful

    Loading HDVPSS Firmware

    FIRMWARE: Memory map bin file not passed

    Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]

    FIRMWARE: Default memory configuration is used

    MemCfg: DCMM (Dynamically Configurable Memory Map) Version :  2.1.1.1

    FIRMWARE: Memory Configuration status : In Progress

    FIRMWARE: 2 start Successful

    open /dev/fb0: No such file or directory

    HDMI W1 rev 2.0

    Timing Info:

     pixel_clk = 148500

     x_res = 1920

     y_res = 1080

     hfp   = 88

     hsw   = 44

     hbp   = 148

     vfp   = 4

     vsw   = 5

     vbp   = 36

    Starting system message bus: dbus.

    Starting telnet daemon.

    Starting syslogd/klogd: done

    Starting thttpd.

    Starting PVR

    /dev/mem opened.

    Memory mapped at address 0x40269000.

    Read at address  0x48180F04 (0x40269f04): 0x00000001

    Write at address 0x48180F04 (0x40269f04): 0x00000000, readback 0x00000000

    /dev/mem opened.

    Memory mapped at address 0x4020b000.

    Read at address  0x48180900 (0x4020b900): 0x00000102

    Write at address 0x48180900 (0x4020b900): 0x00000002, readback 0x00000002

    /dev/mem opened.

    Memory mapped at address 0x402c9000.

    Read at address  0x48180920 (0x402c9920): 0x00040002

    Write at address 0x48180920 (0x402c9920): 0x00000002, readback 0x00000002

    Starting Matrix GUI application.

    _____                    _____           _         _  

    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_

    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|

    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  

                 |___|                    |___|            

    Arago Project http://arago-project.org dm816x-evm ttyO2

    Arago 2011.09 dm816x-evm ttyO2

    dm816x-evm login: root

    root@dm816x-evm:~# ls

    root@dm816x-evm:~# cd /usr/

    /usr/bin/      /usr/include/  /usr/libexec/  /usr/share/

    /usr/games/    /usr/lib/      /usr/sbin/     /usr/src/

    root@dm816x-evm:~# cd /usr/share/

    root@dm816x-evm:/usr/share# cd ti/syslink-examples/

    root@dm816x-evm:/usr/share/ti/syslink-examples# ls

    TI816X

    root@dm816x-evm:/usr/share/ti/syslink-examples# cd TI816X/

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X# ls

    frameq                 listmp                 runsamples_debug.sh

    gatemp                 messageq               runsamples_release.sh

    heapbufmp              notify

    heapmemmp              ringio

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X# cd notify/

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify# ls

    notify_ti81xx_dsp.xe674   run_notifyapp_debug.sh    slaveloader_release

    notifyapp_debug           run_notifyapp_release.sh

    notifyapp_release         slaveloader_debug

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify# /etc/init.d/p

    /etc/init.d/populate-volatile.sh  /etc/init.d/pvr-init

    /etc/init.d/psplash

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify# /etc/init.d/pvr-in

    it stop

    Stopping PVR

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify# /etc/init.d/matrix

    -gui-e stop

    Stopping Matrix GUI application.

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify# /etc/init.d/load-h

    d-firmware.sh stop

    Unloading HDVICP2 Firmware

    FIRMWARE: Memory map bin file not passed

    Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]

    FIRMWARE: Default memory configuration is used

    MemCfg: DCMM (Dynamically Configurable Memory Map) Version :  2.1.1.1

    FIRMWARE: Memory Configuration status : In Progress

    FIRMWARE: 1 stop Successful

    Unloading HDVPSS Firmware

    FIRMWARE: Memory map bin file not passed

    Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]

    FIRMWARE: Default memory configuration is used

    MemCfg: DCMM (Dynamically Configurable Memory Map) Version :  2.1.1.1

    FIRMWARE: Memory Configuration status : In Progress

    FIRMWARE: 2 stop Successful

    Removed syslink kernel module

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify#

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify#

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify# modprobe

    modprobe     modprobe.26

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify# modprobe syslink  

    SysLink version : 2.00.05.85

    SysLink module created on Date:Dec  9 2011 Time:12:47:37

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify#

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify# lsmod

    Module                  Size  Used by

    syslink              1113011  0

    ipv6                  209855  12

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify#

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify#

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify# ls

    notify_ti81xx_dsp.xe674   run_notifyapp_debug.sh    slaveloader_release

    notifyapp_debug           run_notifyapp_release.sh

    notifyapp_release         slaveloader_debug

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify# cat run_notifyapp_

    debug.sh

    #!/bin/sh

    #  

    #   @file   run_notifyapp_debug.sh

    #

    #   @brief  Script to run the debug samples

    #

    #

    #   ============================================================================

    #

    #   Copyright (c) 2008-2009, Texas Instruments Incorporated

    #

    #   Redistribution and use in source and binary forms, with or without

    #   modification, are permitted provided that the following conditions

    #   are met:

    #  

    #   *  Redistributions of source code must retain the above copyright

    #      notice, this list of conditions and the following disclaimer.

    #  

    #   *  Redistributions in binary form must reproduce the above copyright

    #      notice, this list of conditions and the following disclaimer in the

    #      documentation and/or other materials provided with the distribution.

    #  

    #   *  Neither the name of Texas Instruments Incorporated nor the names of

    #      its contributors may be used to endorse or promote products derived

    #      from this software without specific prior written permission.

    #  

    #   THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"

    #   AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,

    #   THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR

    #   PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR

    #   CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,

    #   EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,

    #   PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;

    #   OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,

    #   WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR

    #   OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,

    #   EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

    #   Contact information for paper mail:

    #   Texas Instruments

    #   Post Office Box 655303

    #   Dallas, Texas 75265

    #   Contact information:

    #   www-k.ext.ti.com/.../product-information-centers.htm

    #   DCMP=TIHomeTracking&HQS=Other+OT+home_d_contact

    #   ============================================================================

    #  

    # Run the sample application using the slaveloader method (preferred)

    echo "======== Running app using slaveloader ========"

    ./slaveloader_debug startup DSP ./notify_ti81xx_dsp.xe674

    ./notifyapp_debug

    ./slaveloader_debug shutdown DSP

    # Run the samples application using the optional arguments method to

    # load, run, and stop the slave processor

    echo "======== Running app using agruments ========"

    ./notifyapp_debug 1 DSP ./notify_ti81xx_dsp.xe674

    root@dm816x-evm:/usr/share/ti/syslink-examples/TI816X/notify# ./slaveloader_debu

    g startup DSP ./notify_ti81xx_dsp.xe674

    Attached to slave procId 0.

    BUG: Your driver calls ioremap() on system memory.  This leads

    to architecturally unpredictable behaviour on ARMv6+, and ioremap()

    will fail in the next kernel release.  Please fix your driver.

    ------------[ cut here ]------------

    WARNING: at arch/arm/mm/ioremap.c:211 __arm_ioremap_pfn_caller+0x58/0x190()

    Modules linked in: syslink ipv6 [last unloaded: syslink]

    Backtrace:

    [<c0048b58>] (dump_backtrace+0x0/0x110) from [<c036b8d8>] (dump_stack+0x18/0x1c)

    r7:00000000 r6:c004c678 r5:c0424d8f r4:000000d3

    [<c036b8c0>] (dump_stack+0x0/0x1c) from [<c006bd54>] (warn_slowpath_common+0x54/0x6c)

    [<c006bd00>] (warn_slowpath_common+0x0/0x6c) from [<c006bd90>] (warn_slowpath_null+0x24/0x2c)

    r9:00000002 r8:00000000 r7:bf190b6c r6:0008b000 r5:00026900

    r4:00000000

    [<c006bd6c>] (warn_slowpath_null+0x0/0x2c) from [<c004c678>] (__arm_ioremap_pfn_caller+0x58/0x190)

    [<c004c620>] (__arm_ioremap_pfn_caller+0x0/0x190) from [<c004c834>] (__arm_ioremap_caller+0x64/0x6c)

    [<c004c7d0>] (__arm_ioremap_caller+0x0/0x6c) from [<c005ec6c>] (omap_ioremap+0x60/0x64)

    r6:00000000 r5:00026900 r4:8b000000

    [<c005ec0c>] (omap_ioremap+0x0/0x64) from [<bf190b6c>] (MemoryOS_map+0x1e0/0x398 [syslink])

    r7:cb23fcd8 r6:00000000 r5:cb23fc70 r4:d0807000

    [<bf19098c>] (MemoryOS_map+0x0/0x398 [syslink]) from [<bf15f4d4>] (_ProcMgr_map+0x1cc/0x4a0 [syslink])

    r8:00000001 r7:cb23fcd8 r6:00000000 r5:06a85000 r4:cb23fd54

    [<bf15f308>] (_ProcMgr_map+0x0/0x4a0 [syslink]) from [<bf16d874>] (ElfLoaderTrgWrite_copy+0x13c/0x3a0 [syslink])

    [<bf16d738>] (ElfLoaderTrgWrite_copy+0x0/0x3a0 [syslink]) from [<bf170bf8>] (DLIF_copy+0x18/0x24 [syslink])

    [<bf170be0>] (DLIF_copy+0x0/0x24 [syslink]) from [<bf16f914>] (DLOAD_load+0x834/0xaa8 [syslink])

    [<bf16f0e0>] (DLOAD_load+0x0/0xaa8 [syslink]) from [<bf16cac4>] (ElfLoader_load+0x270/0x330 [syslink])

    [<bf16c854>] (ElfLoader_load+0x0/0x330 [syslink]) from [<bf15d2d0>] (Loader_load+0xec/0x164 [syslink])

    [<bf15d1e4>] (Loader_load+0x0/0x164 [syslink]) from [<bf1618f4>] (ProcMgr_load+0x21c/0x2f8 [syslink])

    [<bf1616d8>] (ProcMgr_load+0x0/0x2f8 [syslink]) from [<bf1639b0>] (ProcMgrDrv_ioctl+0xc8c/0x1cc8 [syslink])

    [<bf162d24>] (ProcMgrDrv_ioctl+0x0/0x1cc8 [syslink]) from [<c00d10e4>] (vfs_ioctl+0x28/0x44)

    r8:bebdeba8 r7:00000007 r6:00000007 r5:cbb4b700 r4:00000000

    [<c00d10bc>] (vfs_ioctl+0x0/0x44) from [<c00d17f4>] (do_vfs_ioctl+0x500/0x540)

    [<c00d12f4>] (do_vfs_ioctl+0x0/0x540) from [<c00d188c>] (sys_ioctl+0x58/0x7c)

    [<c00d1834>] (sys_ioctl+0x0/0x7c) from [<c0044da0>] (ret_fast_syscall+0x0/0x30)

    r8:c0044f48 r7:00000036 r6:00008c58 r5:00000000 r4:00008d04

    ---[ end trace 90dd3005d87f3efb ]---

    Unable to handle kernel paging request at virtual address 00002004

    pgd = cb1f8000

    [00002004] *pgd=8bbaa031, *pte=00000000, *ppte=00000000

    Internal error: Oops: 17 [#1]

    last sysfs file: /sys/module/pvrsrvkm/initstate

    Modules linked in: syslink ipv6 [last unloaded: syslink]

    CPU: 0    Tainted: G        W    (2.6.37 #1)

    PC is at DLOAD_load+0x838/0xaa8 [syslink]

    LR is at ElfLoaderTrgWrite_copy+0x330/0x3a0 [syslink]

    pc : [<bf16f918>]    lr : [<bf16da68>]    psr: 80000013

    sp : cb23fd40  ip : 00000000  fp : cb23fda4

    r10: d586d000  r9 : 0000000b  r8 : 00000001

    r7 : 0000000b  r6 : 00000001  r5 : d587a000  r4 : d58e3000

    r3 : 00002000  r2 : 03046000  r1 : 00060000  r0 : 00000001

    Flags: Nzcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

    Control: 10c5387d  Table: 8b1f8019  DAC: 00000015

    Process slaveloader_deb (pid: 1516, stack limit = 0xcb23e2e8)

    Stack: (0xcb23fd40 to 0xcb240000)

    fd40: cb23fd74 cb23fd50 d586d000 8b03704c 00000000 d586d000 d58e6000 d5a00000

    fd60: 00000001 00000040 00000000 00000002 00000020 d587a000 00000000 d57cd000

    fd80: d57ca000 03046000 00000001 bebdebf8 cb23fec4 d57c7000 cb23fdec cb23fda8

    fda0: bf16cac4 bf16f0ec d586a000 00000001 bebdebf8 00000000 bf18e794 d586d000

    fdc0: cb23fdfc d57c7000 00000001 bebdebf8 d586a000 cb23fec4 d586a000 00000000

    fde0: cb23fe24 cb23fdf0 bf15d2d0 bf16c860 00000000 cb23fec4 bebdebf8 00000000

    fe00: d0a5f000 00000001 d57d9000 bebdebf8 00000000 cb23fec4 cb23fe64 cb23fe28

    fe20: bf1618f4 bf15d1f0 00000000 cb23fec4 bebdebf8 00000000 0000001a 00000000

    fe40: cbb4b700 d586a000 bebdeba8 bf25523c cb23e000 00000000 cb23fef4 cb23fe68

    fe60: bf1639b0 bf1616e4 00000000 cb23fec4 c01d1f8c c01daba0 cb23fe9c cb23fe88

    fe80: c01d1fa8 c01d1f4c 00000000 60000013 caeaaf40 00000000 cb96a400 cb23e000

    fea0: 00000000 0000001c 00000000 d57d9000 bebdee97 0000001a 00000001 bebdebf8

    fec0: 00000000 00000000 cb23fef4 cb23fed8 c01bf340 00000000 cbb4b700 00000007

    fee0: 00000007 bebdeba8 cb23ff04 cb23fef8 c00d10e4 bf162d30 cb23ff74 cb23ff08

    ff00: c00d17f4 c00d10c8 40d16000 caeba580 00000000 00000000 fffffffd 00000000

    ff20: cb23ff54 cb23ff30 c036fa0c c0040170 cc86201c cb84a580 00000017 cc829600

    ff40: cb23e000 00000000 cb23ff6c 00000000 bebdeba8 c020e0a2 00000007 cbb4b700

    ff60: cb23e000 00000000 cb23ffa4 cb23ff78 c00d188c c00d1300 cb23ffac 00000001

    ff80: c036c194 00008d04 00000000 00008c58 00000036 c0044f48 00000000 cb23ffa8

    ffa0: c0044da0 c00d1840 00008d04 00000000 00000007 c020e0a2 bebdeba8 00000007

    ffc0: 00008d04 00000000 00008c58 00000036 00000000 00000000 40114000 bebdeb84

    ffe0: 00000000 bebdeb60 000454ec 401f0aec 60000010 00000007 b470e189 d822d393

    Backtrace:

    [<bf16f0e0>] (DLOAD_load+0x0/0xaa8 [syslink]) from [<bf16cac4>] (ElfLoader_load+0x270/0x330 [syslink])

    [<bf16c854>] (ElfLoader_load+0x0/0x330 [syslink]) from [<bf15d2d0>] (Loader_load+0xec/0x164 [syslink])

    [<bf15d1e4>] (Loader_load+0x0/0x164 [syslink]) from [<bf1618f4>] (ProcMgr_load+0x21c/0x2f8 [syslink])

    [<bf1616d8>] (ProcMgr_load+0x0/0x2f8 [syslink]) from [<bf1639b0>] (ProcMgrDrv_ioctl+0xc8c/0x1cc8 [syslink])

    [<bf162d24>] (ProcMgrDrv_ioctl+0x0/0x1cc8 [syslink]) from [<c00d10e4>] (vfs_ioctl+0x28/0x44)

    [<c00d10bc>] (vfs_ioctl+0x0/0x44) from [<c00d17f4>] (do_vfs_ioctl+0x500/0x540)

    [<c00d12f4>] (do_vfs_ioctl+0x0/0x540) from [<c00d188c>] (sys_ioctl+0x58/0x7c)

    [<c00d1834>] (sys_ioctl+0x0/0x7c) from [<c0044da0>] (ret_fast_syscall+0x0/0x30)

    r8:c0044f48 r7:00000036 r6:00008c58 r5:00000000 r4:00008d04

    Code: e594301c e50b3034 eb0004b2 e594302c (e5932004)

    ---[ end trace 90dd3005d87f3efc ]---

    这是我的log信息