This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: _M4F与A53 Linux进行IPC通讯,M4F端发送数据包长度不能大于256字节

Part Number: AM623


您好,我在测试m4f与a53-linux之间的ipc通讯,我git-clone了ti-rpmsg-char代码(链接https://git.ti.com/cgit/rpmsg/ti-rpmsg-char/)

ti-rpmsg-char代码中稍微修改,重新编译通过。

我将ti-rpmsg-char代码修改成了可以发出任意长度的数据,如下图所示,data_len是一个ssh命令行中获取的发送数据长度,而原代码只能发出"hello there %d"

通过这个程序与m4f进行通讯,m4f端的功能是收到什么内容返回什么内容(有一点我已经明白,发送用户数据不能超过496字节),

如下图所示,当我发送内容小于等于256字节时候,linux可以完整收到m4f端的回复,发送的内容以‘s’开始,以‘e’结束

如下图所示,当我发送内容大于256字节时,linux端就只能收到256字节的数据,发496字节也是返回256字节,发300字节,也是返回256字节,

我通过m4f的串口DebugP_log函数打出了信息,看到m4f是确实收到了所有数据的,且发送的时候也是按收到的长度去传入到RPMessage_send函数进行发送的,

但是就是发不出来,超过256字节就截断。

下图是m4f端vring的配置,vringbuf数量是256个,每个vringbuf长度是512字节(此处已经是512字节,为何出现前文所述的256字节截断问题?)

下面是m4f端的接收发送处部分代码

#define IPC_RPMESSAGE_MAX_MSG_SIZE        (512u)
char recvMsg[IPC_RPMESSAGE_MAX_MSG_SIZE+1]; /* +1 for NULL char in worst case */
    /* wait for messages forever in a loop */
    while(1) {
        /* set 'recvMsgSize' to size of recv buffer,
        * after return `recvMsgSize` contains actual size of valid data in recv buffer
        */
        //DebugP_log("runing task_id=%d localEndPoint=%d rec_cnt=%d\r\n", inputArgs->task_id, localEndPoint, rec_cnt);

        recvMsgSize = IPC_RPMESSAGE_MAX_MSG_SIZE;
        status = RPMessage_recv(pRpmsgObj,
            recvMsg, &recvMsgSize,
            &remoteCoreId, &remoteCoreEndPt,
            0);

        if(status==SystemP_SUCCESS)
        {

            /* echo the same message string as reply */
            #if 1 /* not logging this so that this does not add to the latency of message exchange */
            recvMsg[recvMsgSize] = 0; /* add a NULL char at the end of message */
            //DebugP_log("recvMsg:%s\r\n", recvMsg);
            #endif

            /* send ack to sender CPU at the sender end point */
            status = RPMessage_send(
                recvMsg, recvMsgSize,
                remoteCoreId, remoteCoreEndPt,
                RPMessage_getLocalEndPt(pRpmsgObj),
                5);
            //DebugP_log("Rec Size=%d Cnt=%d ",recvMsgSize, rec_cnt);
            rec_cnt ++;
            if(status==SystemP_SUCCESS)
            {

                //DebugP_log("send ok %d\r\n", send_cnt);
                send_cnt++;
            }
            else
            {
                DebugP_log("send error = %02X\r\n", status);
            }            //DebugP_assert(status==SystemP_SUCCESS);
        }
        else
        {
            vTaskDelay(1);
        }
    }

问题1:上述的问题出在哪里,如何解决

问题2:下图对应的IPC_RPMESSAGE_NUM_VRING_BUF和IPC_RPMESSAGE_MAX_VRING_BUF_SIZE,这两个参数如何理解?

是不是在ipc通讯中,有NUM_VRING个缓存区,每个缓存区的大小是VRING_BUF_SIZE,如果是这样的话,是不是linux连续发送NUM_VRING个消息,m4f一直不读取,一旦启动读取就可以读取出NUM_VRING个消息?

/* Number of a buffers in a VRING, i.e depth of VRING queue */
#define IPC_RPMESSAGE_NUM_VRING_BUF (256U)
/* Max size of a buffer in a VRING */
#define IPC_RPMESSAGE_MAX_VRING_BUF_SIZE (512U)

  • 请看下面e2e工程师的回复。

    请问MCU+ SDK,Linux SDK用的是哪个版本?在SDK 9.0版本里IPC_RPMESSAGE_MAX_MSG_SIZE 最大是496bytes.

    Which versions of the MCU+ SDK and the Linux SDK are the customer using?

    We accidentally placed a limitation on the size of the RPMsg message that the M4F would receive in earlier MCU+ SDK examples for Linux RPMsg. So the M4F code is the first place I would look.

    e.g., if I check MCU+ SDK 8.3, file examples/drivers/ipc/ipc_rpmsg_echo_linux/ipc_rpmsg_echo.c

    I see
    /* maximum size that message can have in this example */
    #define IPC_RPMESSAGE_MAX_MSG_SIZE (96u)

    while if we check MCU+ SDK 9.0, file examples/drivers/ipc/ipc_rpmsg_echo_linux/ipc_rpmsg_echo.c
    I see
    /* Maximum size that message can have in this example
    * RPMsg maximum size is 512 bytes in linux including the header of 16 bytes.
    * Message payload size without the header is 512 - 16 = 496
    */
    #define IPC_RPMESSAGE_MAX_MSG_SIZE (496u)

    As far as IPC_RPESSAGE_NUM_VRING_BUF and IPC_RPESSAGE_MAX_VRING_BUF_SIZE:

    IPC_RPESSAGE_NUM_VRING_BUF - this is the number of RPMsg messages that can be queued up in each direction (i.e., 256 from Linux to M4F, and 256 from M4F to Linux, for a total of 512 VRING buffers total)

    IPC_RPESSAGE_MAX_VRING_BUF_SIZE - this should stay at 512 bytes total per VRING buffer.

  • TI还有一个zerocopy的demo,你可以看一下,适用于传输大量的数据

    git.ti.com/.../