背景:由于使用的是自己做的6678的板子,因此DDR3布线与EVM略有出入,DDR3无法运行在1333速率,只能运行在1066速率。
现在想要在板子上实现Nor flash boot,因此尝试使用MCSDK提供的norwriter_evm6678l例程,按照论坛上提供的方法,进行程序烧写。而该例程的CCS启动用到DDR3,需要使用gel文件,对DDR3做初始化。因此自己尝试去修改gel中DDR3 PLL配置段代码。但是发现该段代码如下:
/****************************************************************************
*
* NAME
* Set_Pll2_666_7_MHz
*
* PURPOSE:
* Setup PLL 2 DDR @ 666.7 MHz with External clock
*
* USAGE
* This routine can be called as:
*
* Set_Pll2_666_7_MHz()
*
* RETURN VALUE
* NONE
*
* REFERENCE
*
****************************************************************************/
hotmenu Set_Pll2_666_7_MHz( )
{
Set_Pll2();
}
而Set_Pll2()函数我无法找到,因此不知道如何修改?
请问有办法能够修改gel文件中DDR3 PLL的配置么?