由于工程需要,需要使用两块C6414的McBSP借口进行互联高速通信,DSP的McBSP0串口按照规定步骤进行初始化,每次传送一幁128个32bit的数据,使用EDMA进行触发传输。DSP刚上电后即进行传输,由于串口的多级缓存,上电后的初始状态能看到DX0和DR0均为0,发送端使用EDMA发送了128个数据,但是接收端只能收到127个数据,无法达到设置的EDMA接受128个数据的设置,故无法触发EDMA完毕中断,最后一个数据在发送端的DX0内。如果程序再次用CCS加载,由于此时DX0的数据不为空,接收端可以完整接受128个数据触发EDMA中断。需要如何设置才能使初次加电后能确保发送端完整发送,接收端完整接受呢?