Part Number: TMS320C6678
通过网上资料得知:DSP供电正常、时钟稳定后,驱动RESET、POR、RESETFULL依次拉高。请问推荐的上电时序是CVDD→1.0V→1.8V→1.5V→3.3V,还是3.3V→CVDD→1.0V→1.8V→1.5V?时钟发生器是3.3V供电的。3.3V先于CVDD是否会有问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6678
通过网上资料得知:DSP供电正常、时钟稳定后,驱动RESET、POR、RESETFULL依次拉高。请问推荐的上电时序是CVDD→1.0V→1.8V→1.5V→3.3V,还是3.3V→CVDD→1.0V→1.8V→1.5V?时钟发生器是3.3V供电的。3.3V先于CVDD是否会有问题?
TMS320C6678没有3.3v供电的,上电顺序有两种,请参考数据手册。
7.3.1 Power-Supply Sequencing
https://www.ti.com/lit/ds/symlink/tms320c6678.pdf
电源设计,可以参考下面的应用文档。
2 Power Supplies
https://www.ti.com/lit/an/sprabi2d/sprabi2d.pdf
外设是3.3v电平的话,是需要电平转换芯片成1.8v后,才能和DSP相连。
如果是时钟发生器,输入时钟是要在电源稳定后才能给DSP,请看数据手册上的说明。
The clock input buffers for CORECLK, DDRCLK, PASSCLK, SRIOSGMIICLK, PCIECLK and MCMCLK use CVDD as a supply voltage. These clock inputs are not failsafe and must be held in a high-impedance state until CVDD is at a valid voltage level. Driving these clock inputs high before CVDD is valid could cause damage to the device.