Part Number: PROCESSOR-SDK-AM64X
Other Parts Discussed in Thread: SYSCONFIG
我这边现在运行网络模块的例程,所有的例程(例如C:\ti\mcu_plus_sdk_am64x_09_01_00_41\examples\networking\lwip\enet_cpsw_socket)必须把I2C Address这里更改为0x68程序才能运行,否则报错
Enabling clocks!
Assertion @ Line: 364 in syscfg/ti_board_config.c: ENET_GET_NUM_MAC_ADDR(numMacMax) <= ENET_BOARD_NUM_MACADDR_MAX : failed !!!
但是这个地方按照我的理解应该是EEPROM的地址,那么他的地址就是0X50,而0x68是RTC的位置,而且所有的例程都是用的0x50,我这边运行例程C:\ti\mcu_plus_sdk_am64x_09_01_00_41\examples\drivers\i2c\i2c_read读取0x50的数据是正常的
1 为什么我在网络模块中用0x50不行?
2 如果我用0x68会不会对我的程序有影响?