This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: AM623的Main_SPI0作为主机,FPGA作为从机,能否达到20ms 128*32 byte

Part Number: AM623


AM623的Main_SPI0作为主机,FPGA作为从机,通过中断的方式,能否达到20ms 128*32 byte呢?目前打算通过GPIO中断直接进行SPI读写数据,然后通过DMA给到内存,请问这个方案有什么问题吗?如果可以实现能否提供下这个方案实现上的帮助呢?例如:Main_SPI0如何配置为DMA模式,还有如何操作可以通过GPIO中断实现SPI数据读写呢?