This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM620-Q1: 软件问题咨询

Part Number: AM620-Q1
Other Parts Discussed in Thread: AM62A3-Q1

Hi TI expert

有以下问题需要麻烦您帮助确认:

1、开发板的双千兆网口是否提供在a53核上基于rtos或者裸跑的bsp

2、开发板上的LPDDR4是否提供在a53核上基于rtos或者裸跑的控制

3、AM62A3-Q1上的spi,i2c,uart,can-fd是否提供在a53核上基于rtos或者裸跑的bsp,thanks

1. Whether the dual Gigabit network port of the development board provides rtos or bare-run bsp on the a53 core
2. Whether the LPDDR4 on the development board provides RTOs-based or bare run control on the a53 core
3. Whether spi, i2c, uart, can-fd on AM62A3-Q1 provide rtos or bare-run bsp on a53 core