大家好,本人现在做的项目需要DSP上拥有两个千兆以太网,查询型号时发现C6472和C667X系列都满足要求,但是C667X说是拥有两个SGMII接口和一个SWITCH,和C6472拥有两个EMAC在功能上有什么不一样呢?还有既然都是多核,那么C6472和C667X系列之间还有什么区别呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,本人现在做的项目需要DSP上拥有两个千兆以太网,查询型号时发现C6472和C667X系列都满足要求,但是C667X说是拥有两个SGMII接口和一个SWITCH,和C6472拥有两个EMAC在功能上有什么不一样呢?还有既然都是多核,那么C6472和C667X系列之间还有什么区别呢?
c6472是C64x+的核,C667x是C66的核;同样频率下C66性能更好且支持浮点;
EMAC口都可以支持两个千兆以太,对外功能基本一致,C667x拥有的switch和NETCP可以实现更多的功能如包的过滤;
C6472是65nm的工艺,C667x是40nm工艺;
如果现在选择,建议是C667x系列
那是不是C6472和C667X的EVM板都具有两个Ethernet接口?而且能同时工作?包的过滤这一块能详细说一下吗?或者能告诉我看哪个文件?因为我做的一部分功能是IP过滤
关于667x的技术文档都在http://www.ti.com/product/TMS320C6678/technicaldocuments,
6472和667x的EVM并没有设置两个Ethernet接口,主要是出于EVM的成本考虑;包的过滤你可以看看667X的Network Coprocessor和Packet Accelerator的User Guide