This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730 Camera ISP CCDC Status Checking

Other Parts Discussed in Thread: TVP5146, AM4378

请教个问题,关于CCDC的busy状态, The CCDC_PCR 1] BUSY status bit is set when the start of frame occurs (if the CCDC_PCR[0] ENABLE
bit is 1 at that time). It is automatically reset to 0 at the end of a frame. 手册上是这样说的,那么使用bt656模式时,如何判断帧的开始和结束?

我使用tvp5146采集pal60制式,bt656的数据流,出现如下信息

[    6.003845] ccdc_vd0_isr     fid 8000 cnt 66
[    6.020507] ccdc_vd0_isr     fid 0 cnt 67
[    6.026275] omap3isp omap3isp: CCDC won't become idle!
[    6.037231] ccdc_vd0_isr     fid 8000 cnt 68
[    6.053894] ccdc_vd0_isr     fid 0 cnt 69
[    6.059661] omap3isp omap3isp: CCDC won't become idle!

能够识别奇偶场,但是区分不了帧

  • bt656是内嵌同步,具体的看同步,可以查看 http://www.360doc.com/content/10/0910/14/3267359_52627520.shtml 

    DM37的摄像头口目前的支持比较有限,如果您的项目刚开始,建议您看看http://www.ti.com/product/AM4378/toolssoftware#softTools 

  • In the case of BT.656 input mode, there is VS at the beginning of each field. Therefore,
    there are two interrupts for each frame (one for each field)

    这才是我要的