This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730仿真器与开发板连接错误

Other Parts Discussed in Thread: DM3730

用的是CCS5.5,在连接仿真器的时候时,提示:

[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -v -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\123\AppData\Local\.TI\3438098274\
0\0\BrdDat\testBoard.dat
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'AH510plusV5.dll'.
The library build date was 'Aug 20 2013'.
The library build time was '22:56:19'.
The library package version is '5.1.232.0'.
The library component version is '35.34.40.0'.
5ac3 5ac3
a77c a53c
0f4f 0f0f
3ee5 3ca5
c35a c35a

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-171' (0xffffff55).
The title is 'SC_ERR_REG_DETECT_CTLR'.

The explanation is:
The wrong controller address value has been used.
A controller cannot be detected even though the
selected port does match the hardware configuration.

[End]

请问是什么原因?该怎么解决?另外请教一下DM3730  DSP是否可以对I/O口外设直接操作。