This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: AM6442 EVM:A53运行linux和R5F,M4核心通信

Part Number: AM6442


利用linux来和R5,M4做ipc通信,更改官方的例程rpmsg_char_simple.c之后如何编译,编译一直没法通过

/usr/lib/gcc/aarch64-linux/9.2.1/../../../../aarch64-linux/bin/ld: /tmp/ccygnyZN.o: in function `rpmsg_char_ping':
rpmsg_char_simple.c:(.text+0x150): undefined reference to `rpmsg_char_open'
/usr/lib/gcc/aarch64-linux/9.2.1/../../../../aarch64-linux/bin/ld: rpmsg_char_simple.c:(.text+0x308): undefined reference to `rpmsg_char_close'
/usr/lib/gcc/aarch64-linux/9.2.1/../../../../aarch64-linux/bin/ld: /tmp/ccygnyZN.o: in function `main':
rpmsg_char_simple.c:(.text+0x4b0): undefined reference to `rpmsg_char_init'
/usr/lib/gcc/aarch64-linux/9.2.1/../../../../aarch64-linux/bin/ld: rpmsg_char_simple.c:(.text+0x4f4): undefined reference to `rpmsg_char_exit'
collect2: error: ld returned 1 exit status

这是报错

  • 官方例程不建议修改~

    如您修改了官方示例代码后,需要确保以下几点:

    1. 您的修改没有错误,并且正确地调用了所需的函数
    2. 您包含了正确的头文件,编译器知道函数的声明
    3. 您链接了所需的库或对象文件