This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6657: 在-20摄氏度环境下运行会自动降低功率吗?

Part Number: TMS320C6657

用TMS320C6657作为CPU,在常温条件下运行试验,每10毫秒采集一帧正弦波并显示。这个正常。

但在-20摄氏度环境下运行试验,当运行4小时后,采集就会出现异常,感觉什么芯片运行速度变慢了一样。

我用的是扩展温度型号,即-40℃——100℃,那么在-20℃下会降低功效吗?

x 出现错误。请重试或与管理员联系。