This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x双网口划vlan



我用的是米尔的核心板,sd启动,以下是打印的启动信息,


U-Boot SPL 2011.09 (Apr 14 2014 - 15:45:47)
Texas Instruments Revision detection unimplemented
Booting from MMC...
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img


U-Boot 2011.09 (Apr 14 2014 - 15:45:47)

I2C:   ready
DRAM:  512 MiB
WARNING: Caches not enabled
Did not find a recognized configuration, assuming General purpose EVM in Profile 0 with Daughter board
NAND:  HW ECC Hamming Code selected
512 MiB
MMC:   OMAP SD/MMC: 0
Net:   cpsw
Hit any key to stop autoboot:  3 2 1 0
sysboot[4-0]: 0x16 ... sdboot.
SD/MMC found on device 0
reading uEnv.txt

** Unable to read "uEnv.txt" from mmc 0:1 **
reading uImage

3619144 bytes read
reading ramdisk.gz

** Unable to read "ramdisk.gz" from mmc 0:1 **
Booting from nand ...
HW ECC BCH8 Selected

NAND read: device 0 offset 0x280000, size 0x400000
 4194304 bytes read: OK
## Booting kernel from Legacy Image at 80007fc0 ...
   Image Name:   Linux-3.2.0
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3604432 Bytes = 3.4 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   XIP Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Linux version 3.2.0 (lihacker@lihacker-laptop) (gcc version 4.4.1 (Sourcery G++ Lite 2010q1-202) ) #28 Fri Jan 30 16:03:09 CST 2015
CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: am335xevm
Memory policy: ECC disabled, Data cache writeback
AM335X ES1.0 (sgx neon )
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
Kernel command line: console=ttyO0,115200n8 board-am335xevm.display_mode=lcd7ir root=ubi0:rootfs rw ubi.mtd=7,2048 noinitrd rootfstype=ubifs rootwait=1 ip=none
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 512MB = 512MB total
Memory: 512512k/512512k available, 11776k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)
    lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    modules : 0xbf000000 - 0xc0000000   (  16 MB)
      .text : 0xc0008000 - 0xc063b000   (6348 kB)
      .init : 0xc063b000 - 0xc067b000   ( 256 kB)
      .data : 0xc067c000 - 0xc06e4730   ( 418 kB)
       .bss : 0xc06e4754 - 0xc0711924   ( 181 kB)
NR_IRQS:396
IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
Total of 128 interrupts on 1 active controller
OMAP clockevent source: GPTIMER2 at 24000000 Hz
omap_dm_timer_switch_src: Switching to HW default clocksource(sys_clkin_ck) for timer1, this may impact timekeeping in low power state
OMAP clocksource: GPTIMER1 at 24000000 Hz
sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
Console: colour dummy device 80x30
Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
omap_hwmod: pruss: failed to hardreset
print_constraints: dummy:
NET: Registered protocol family 16
OMAP GPIO hardware version 0.1
omap_mux_init: Add partition: #1: core, flags: 0
The board is MYD-AM335X.
 omap_hsmmc.0: alias fck already exists
 davinci-mcasp.0: alias fck already exists
--------uart1_init
--------uart2_init
--------uart3_init
--------uart4_init
 d_can.1: alias fck already exists
_omap_mux_get_by_name: Could not find signal mii1_refclk.gpio0_29
registered am33xx_sr device
 omap2_mcspi.1: alias fck already exists
 omap2_mcspi.2: alias fck already exists
 edma.0: alias fck already exists
 edma.0: alias fck already exists
 edma.0: alias fck already exists
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done Qmgr-base(e087a000) dma-base(e0878000)
Cppi41 Init Done
musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource gp timer
musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
MUSB0 controller's USBSS revision = 4ea20800
musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
MUSB1 controller's USBSS revision = 4ea20800
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
usb usb1: SerialNumber: musb-hdrc.1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using DMA, IRQ 19
NET: Registered protocol family 2
IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
TCP established hash table entries: 16384 (order: 5, 131072 bytes)
TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
NetWinder Floating Point Emulator V0.97 (double precision)
omap-gpmc omap-gpmc: GPMC revision 6.0
Registering NAND on CS0
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
msgmni has been set to 1001
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
console [ttyO0] enabled
omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[drm] Initialized drm 1.1.0 20060810
brd: module loaded
loop: module loaded
i2c-core: driver [tsl2550] using legacy suspend method
i2c-core: driver [tsl2550] using legacy resume method
mtdoops: mtd device (mtddev=name/number) must be supplied
omap2-nand driver initializing
ONFI flash detected
ONFI param page 0 valid
NAND device: Manufacturer ID: 0xad, Chip ID: 0xdc (Hynix H27U4G8F2DTR-BC)
Creating 8 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "SPL"
0x000000020000-0x000000040000 : "SPL.backup1"
0x000000040000-0x000000060000 : "SPL.backup2"
0x000000060000-0x000000080000 : "SPL.backup3"
0x000000080000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x000000780000 : "Kernel"
0x000000780000-0x000020000000 : "File System"
OneNAND driver initializing
UBI: attaching mtd7 to ubi0
UBI: physical eraseblock size:   131072 bytes (128 KiB)
UBI: logical eraseblock size:    126976 bytes
UBI: smallest flash I/O unit:    2048
UBI: sub-page size:              512
UBI: VID header offset:          2048 (aligned 2048)
UBI: data offset:                4096
UBI: max. sequence number:       206
UBI: attached mtd7 to ubi0
UBI: MTD device name:            "File System"
UBI: MTD device size:            504 MiB
UBI: number of good PEBs:        4032
UBI: number of bad PEBs:         4
UBI: number of corrupted PEBs:   0
UBI: max. allowed volumes:       128
UBI: wear-leveling threshold:    4096
UBI: number of internal volumes: 1
UBI: number of user volumes:     1
UBI: available PEBs:             0
UBI: total number of reserved PEBs: 4032
UBI: number of PEBs reserved for bad PEB handling: 40
UBI: max/mean erase counter: 3994/3992
UBI: image sequence number:  43703682
UBI: background thread "ubi_bgt0d" started, PID 574
CAN device driver interface
CAN bus driver for Bosch D_CAN controller 1.0
d_can d_can.1: device registered (irq=55, irq_obj=56)
davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
davinci_mdio davinci_mdio.0: detected phy mask ffffffaf
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[4]: device 0:04, driver unknown
davinci_mdio davinci_mdio.0: phy[6]: device 0:06, driver unknown
PPP generic driver version 2.4.2
PPP BSD Compression module registered
PPP Deflate Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
usbcore: registered new interface driver zd1201
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver cdc_eem
usbcore: registered new interface driver dm9601
cdc_ncm: 04-Aug-2011
usbcore: registered new interface driver cdc_ncm
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
 gadget: using random self ethernet address
 gadget: using random host ethernet address
usb0: MAC 22:2c:f9:ff:3b:b7
usb0: HOST MAC 42:e5:c4:72:c1:1c
 gadget: Ethernet Gadget, version: Memorial Day 2008
 gadget: g_ether ready
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: MUSB HDRC host driver
usb usb2: Manufacturer: Linux 3.2.0 musb-hcd
usb usb2: SerialNumber: musb-hdrc.0
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
_regulator_get: deviceless supply vdd_mpu not found, using dummy regulator
cpuidle: using governor ladder
cpuidle: using governor menu
omap4_aes_mod_init: loading AM33X AES driver
omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
omap4_aes_probe: probe() done
omap4_sham_mod_init: loading AM33X SHA/MD5 driver
omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
omap4_sham_probe: probe() done
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
ALSA device list:
  No soundcards found.
oprofile: hardware counters not available
oprofile: using timer interrupt.
nf_conntrack version 0.5.0 (8008 buckets, 32032 max)
ip_tables: (C) 2000-2006 Netfilter Core Team
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
ThumbEE CPU extension supported.
mux: Failed to setup hwmod io irq -22
Power Management for AM33XX family
Trying to load am335x-pm-firmware.bin (60 secs timeout)
Copied the M3 firmware to UMEM
Compensating OPP0 for 0mV Orig nvalue:0x99c0ac New nvalue:0x99c0ac
Compensating OPP1 for 0mV Orig nvalue:0x9a8cfb New nvalue:0x9a8cfb
_regulator_get: deviceless supply vdd_core not found, using dummy regulator
smartreflex smartreflex: am33xx_sr_probe: cannot determine opp
smartreflex: probe of smartreflex failed with error -22
sr_init: platform driver register failed
clock: disabling unused clocks to save power
Detected MACID=88:33:14:f6:af:68
cpsw: Detected MACID = 88:33:14:f6:af:6a
input: gpio-keys as /devices/platform/gpio-keys/input/input0
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
UBIFS: recovery needed
mmc0: host does not support reading read-only switch. assuming write-enable.
mmc0: new SD card at address c914
mmcblk0: mmc0:c914 SU02G 1.84 GiB
 mmcblk0: p1
UBIFS: recovery completed
UBIFS: mounted UBI device 0, volume 0, name "rootfs"
UBIFS: file system size:   504983552 bytes (493148 KiB, 481 MiB, 3977 LEBs)
UBIFS: journal size:       9023488 bytes (8812 KiB, 8 MiB, 72 LEBs)
UBIFS: media format:       w4/r0 (latest is w4/r0)
UBIFS: default compressor: lzo
UBIFS: reserved for root:  0 bytes (0 KiB)
VFS: Mounted root (ubifs filesystem) on device 0:13.
Freeing init memory: 256K
udevd (892): /proc/892/oom_adj is deprecated, please use /proc/892/oom_score_adj instead.
net eth0: CPSW phy found : id is : 0x4dd072
input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input1
net eth1: CPSW phy found : id is : 0x4dd072
Disabling lock debugging due to kernel taint
HSM4B modules is install
register_chrdev is success!

.-------.                                          
|       |                  .-.                     
|   |   |-----.-----.-----.| |   .----..-----.-----.
|       |     | __  |  ---'| '--.|  .-'|     |     |
|   |   |  |  |     |---  ||  --'|  |  |  '  | | | |
'---'---'--'--'--.  |-----''----''--'  '-----'-'-'-'
                -'  |
                '---'

The Angstrom Distribution tips ttyO0

Angstrom 2008.1-test-20090127 tips ttyO0

tips login: root
login[3162]: root login  on `ttyO0'


root@mier:~#

make menuconfig配置如图